1.4 ADC User Sequence
This example application shows how to sample three analog inputs using the user sequencer in external trigger mode (TC peripheral) and send the converted data to the console.
Description
Conversion of the three analog inputs is triggered by TC peripheral at every 500 ms. The user sequencer is used to define the order of conversion:
| Board | Sequence of conversion |
|---|---|
| SAMA7D65 Curiosity Board | MPLABX project for SAMA7D65 Curiosity Board |
| SAMA7D65 Curiosity Pro Board | MPLABX project for SAMA7D65 Curiosity Pro Board |
Analog input voltage in the range of 0V to 3.3V is fed to the ADC input channel AD0, AD3 and AD1. ADC conversion result is displayed on the console.
Downloading and Building the Application
To clone or download this application from Github, go to the main page of this repository and then click Clone button to clone this repository or download as zip file. This content can also be downloaded using content manager by following these instructions.
Path of the application within the repository is apps/adc/adc_user_sequence .
To build the application, refer to the following table and open the project using its IDE.
| Project Name | Description |
|---|---|
| sam_a7d65_curiosity.X | MPLABX project for SAMA7D65 Curiosity Board |
| sam_a7d65_curiosity_pro.X | MPLABX project for SAMA7D65 Curiosity Pro Board |
Setting Up AT91Bootstrap Loader
To load the application binary onto the target device, we need to use at91bootstrap loader. Refer to the at91bootstrap loader documentation for details on how to configure, build and run bootstrap loader project and use it to bootstrap the application binaries.
Setting Up the Hardware
The following table shows the target hardware for the application projects.
| Project Name | Description |
|---|---|
| sam_a7d65_curiosity.X | SAMA7D65 Curiosity Board |
| sam_a7d65_curiosity_pro.X | SAMA7D65 Curiosity Pro Board |
Setting Up SAMA7D65 Curiosity Board
- Connect the USBA port J3 on the board to the computer using a Type-C USB cable (to power the board)
- Connect the UART Debug port (J35) on the board to the computer using a FTDI-USB cable
- Use a jumper wire to connect Pin 11 of RPi connector (AD0 is mapped to Port Pin PC3) to 3.3V or GND
- Use a jumper wire to connect Pin 13 of RPi connector (AD1 is mapped to Port Pin PC4) to 3.3V or GND
- Use a jumper wire to connect Pin 5 of RPi connector (AD3 is mapped to Port Pin PC6) to 3.3V or GND
Setting Up SAMA7D65 Curiosity Pro Board
- Connect the USBA port J1 on the board to the computer using a Type-C USB cable (to power the board)
- Connect the UART Debug port (J63) on the board to the computer using a FTDI-USB cable
- Use a jumper wire to connect Pin 11 of RPi connector (AD0 is mapped to Port Pin PC3) to 3.3V or GND
- Use a jumper wire to connect Pin 13 of RPi connector (AD1 is mapped to Port Pin PC4) to 3.3V or GND
- Use a jumper wire to connect Pin 5 of RPi connector (AD3 is mapped to Port Pin PC6) to 3.3V or GND
Running the Application
- Build the application using its IDE.
- Open the Terminal application (Ex.: Tera term) on the computer.
- Connect to the Virtual COM port and
configure the serial settings as follows:
- Baud: 115200
- Data: 8 Bits
- Parity: None
- Stop: 1 Bit
- Flow Control: None
- The console displays the ADC Count and
the ADC Input Voltage.