The following are the steps to select the new RNBD350 firmware:
Turn on mobile Bluetooth®, and open the MBD application.
As shown in the consoletext log, the
user must establish a connection from the MBD app.
By default, the RNBD350 is programmed to behave in the Data
mode, where the device advertises during power-up. The devices that advertise the
Bluetooth Low Energy packets are called peripheral devices. Each peripheral device
has a unique advertising name. The mobile acts as a Bluetooth Low Energy central
device, scans the surrounding Bluetooth Low Energy advertisements and lists all the
available devices in the scan list.
Tap OTA DFU in the MBD application.
Select the RNBD350_XXXX from the scan
list (XXXX means the last two bytes of the device BD address). Figure 8-25. Microchip Bluetooth Data
OTA DFU Interface
The central device (mobile
application) now gets connected with the device, and connection-related logs are
visible on the tools’ console. Figure 8-26. RNBD350 Device Connection
Log in Microchip RNBD Utility Tool Terminal
When connected, tap Select
Image to choose the available firmware file. The OTAU firmware image file
copied in step 4 is visible on the screen. Figure 8-27. Microchip Bluetooth Data
OTA DFU Firmware Image SelectionUpon selecting the image shown above, the below selection displays. Figure 8-28. Microchip Bluetooth Data
App OTA DFU Browse Firmware Image
After confirmation of the firmware version, click OK to continue. Figure 8-29. Microchip Bluetooth Data
DFU OTA Firmware Version Confirmation
The firmware receipt is initiated and displayed in the console log and mobile app,
which represents the status of the procedure's progress. Figure 8-30. Firmware Update in Progress: MBD OTA DFU ViewFigure 8-31. Microchip RNBD Utility Tool OTA DFU Firmware Image Receive in
Progress
The mobile application and the Microchip Utility Tool display confirmation messages
about the successful OTA firmware receipt: “OTA update successful” and “Received
complete firmware data”. Figure 8-32. Microchip RNBD Utility Tool OTA DFU Firmware Image Receive
CompleteFigure 8-33. MBD OTA DFU Firmware Receive CompleteFigure 8-34. MBD OTA DFU Firmware Receive Complete
After successfully receiving the OTA
firmware, The Bluetooth Low Energy connection with the MBD app will disconnect and
will proceed with the serial DFU update. Click OK in the pop-up dialog. Figure 8-35. Microchip RNBD Utility
Tool OTA DFU Firmware Image Receive Completed
During the firmware update, the tool
displays the following information:
Progress label that displays
the percentage of completion
After clicking OK, the console
text log displays the total time taken for the firmware update along with the “HOST
OTA Successful” message. Figure 8-38. Microchip RNBD Utility
Tool OTA DFU Tab Firmware Update Complete Time
DS50003684B
The online versions of the documents are provided as a courtesy. Verify all content and data in the device’s PDF documentation found on the device product page.