3.2.1 Setting up the Hardware for PolarFire DisplayPort Tx
To set up the hardware for the PolarFire DisplayPort Tx, perform the following steps:
- Connect the DisplayPort daughter card to J14 of the FMC connector of the PolarFire Video kit.
- Connect the DisplayPort cable to the DisplayPort Tx on the DisplayPort FMC daughter card.
- Connect the Host PC and the video kit using the USB mini cable through J12 on the video kit.
- Connect the 12V power supply cable to the J20 onboard DC jack on the video kit.
- Ensure that the jumper settings on the video kit are correctly configured according to the preceding table.
- Power-up the board using the SW4 slide switch.
- After the powering up, program the PolarFire Video kit device. For more information, see Programming the PolarFire Device using FlashPro Express.
- Once the PolarFire device is programmed, the live feed starts streaming the camera video data.