5 Appendix 2 - DDR3 Configuration
(Ask a Question)If you are using Rev F kit, the following are the configurations for DDR3 controller with the initialization and timing parameters for MT41K512M8DA-107: P part present on the Rev F PolarFire Evaluation kit.
- On General tab, set CCC PLL Clock Multiplier to 8, DQ Width as 16, and Column Address Width as 10, as shown in following figure. The clock multiplier value of 8 sets the CCC PLL reference clock frequency to 83.333 MHz.
A reference clock of this frequency is required for the PLL present inside the DDR3 subsystem. The PLL generates a 666.666 MHz DDR3 memory clock frequency and a 166.666 MHz DDR3 AXI clock frequency. The DQ Width is set to 16 to match the width of the DDR3 memory present on the board.
Figure 5-1. General Tab - On the Memory Initialization tab, set the initialization configuration settings for the DDR3 memory as shown in the following figure.
Figure 5-2. Memory Initialization 
- On the Memory Timing tab, set the timing configuration settings for the DDR3 memory as shown in the following figure.
Figure 5-3. Memory Timing 
- On the Controller tab, set the controller configuration settings for the DDR3 memory as shown in the following figure.
Figure 5-4. Controller 
- On the Misc. tab, set the miscellaneous configuration settings for the DDR3 memory as shown in the following figure.
Figure 5-5. Misc