7 Revision History

The revision history describes the changes that were implemented in the document. The changes are listed by revision, starting with the current publication.

Table 7-1. Revision History
RevisionDateDescription
C01/2025The following is a summary of the changes made in revision C of this document.
B07/2024The following is a summary of the changes made in revision B of this document.
A06/2023The following is a summary of the changes made in revision A of this document.
  • Document migrated from Microsemi template to Microchip template.
  • Document number was changed to DS-00004997A from TU0775.
  • Updated the document for Libero v2023.1.
9.0—The following is a summary of the changes made in this revision.
8.0—The following is a summary of the changes made in this revision.
7.0—The following is a summary of the changes made in this revision.
  • Updated Figure 1-1.
  • Replaced Figure 2-4.
  • Removed sections Instantiating On-chip SRAM, Instantiating the AXI3 to AHB-Lite Bridge, Instantiating the AHB-Lite Bus, and Instantiating the AHB-Lite to APB3 Bridge.
  • Updated section Connecting IP Instances in SmartDesign.
6.0—Updated for Libero SoC v12.5.
5.0—The following is a summary of the changes made in this revision.
  • Updated for Libero SoC v12.2.
  • Updated the design for AXI-based Mi-V Soft Processor for an enhanced performance with DDR memories.
  • Removed Libero SoC and SoftConsole version numbers.
4.0—The following is a summary of the changes made in this revision.

Added Fabric RAMs Initialization.

The document was updated for Libero SoC v12.0.

3.0—The following is a summary of the changes made in this revision.
  • Added Design Description.
  • The document was updated for Libero SoC PolarFire v2.1.
2.0—The following is a summary of the changes made in this revision.

The document was updated for the Mi-V processor upgrade.

The document was updated for Libero SoC PolarFire v2.0 and SoftConsole v5.2. For more information, see Building the User Application Using SoftConsole.

Information about TCM initialization from external SPI flash was added. For more information, see Configure Design Initialization Data and Memories.

1.0—The first publication of this document.