4 Appendix 1: Programming the Device using FlashPro Express
(Ask a Question)This chapter describes how to program the PolarFire device with the Job
programming file using a FlashPro programmer. The default location of the
.job file is:
mpf_an4997_df\Programming_files
To program the PolarFire device using FP Express, perform the following steps:
- Ensure that the jumper settings on the board are the same as listed in Table 2-4.Important: Switch off the power supply while making the jumper connections.
- Connect the power supply cable to the J9 connector on the board.
- Connect the USB cable from the Host PC to the J5 (FTDI port) on the board.
- Power ON the board using the SW3 slide switch.
- On the host PC, launch the FlashPro Express software.
- To create a new job project, click New or select New Job Project from Project menu.
- Enter the following in the Create New Job Project dialog box:
- Import FlashPro Express job file: Click
Browse, and navigate to the location where the
.jobfile is located and select the file. The default location is: <download_folder>\mpf_an4997_df\Programming_files.- mpf_an4997_df\Programming_files\top_RevD
- mpf_an4997_df\Programming_files\top_RevF
- FlashPro Express job project location: Click Browse and navigate to the location where you want to save the project.
Figure 4-1. New Job Project from FlashPro Express Job
- Import FlashPro Express job file: Click
Browse, and navigate to the location where the
- Click OK. The required programming file is selected and ready to be programmed in the device.
- The FlashPro Express window appears as shown in the following figure. Confirm that a programmer number appears in the Programmer field. If it does not, confirm the board connections and click Refresh/Rescan Programmers.
Figure 4-2. Programming the Device - Click RUN. When the device is programmed successfully, a RUN PASSED status is displayed as shown in the following figure.
Figure 4-3. FlashPro Express—RUN PASSED - Close FlashPro Express or in the Project tab, click Exit.