An external voltage instead of the on-board target regulator can power the PIC18F57Q43 Curiosity Nano. When the Voltage Off (VOFF) pin is
            shorted to ground (GND), the on-board debugger firmware disables the target regulator,
            and it is safe to apply an external voltage to the VTG pin.
        It is also safe to apply an external voltage to the VTG pin when no USB cable is plugged
            into the DEBUG connector on the board.
        The VOFF pin can be tied low/let go at any time. This will be detected by a
            pin-change interrupt to the on-board debugger, which controls the target voltage
            regulator accordingly.
        Warning: Applying an external
            voltage to the VTG pin without shorting VOFF to GND may cause permanent damage to the
            board.
        Warning: Do not apply any voltage
            to the VOFF pin. Let the pin float to enable the power supply.
        Warning: The absolute maximum
            external voltage is 5.5V for the on-board level shifters, and the standard operating
            condition of the PIC18F57Q43 is 1.8-5.5V. Applying a higher voltage may cause permanent damage to the
            board.
        Info: If an
            external voltage is applied without pulling the VOFF pin low and an external supply
            pulls the voltage lower than the monitoring window’s lower limit (target voltage setting
            – 100 mV), the on-board debugger status LED will blink rapidly and shut the on-board
            regulator off. If an external voltage is suddenly removed when the VOFF pin is not
            pulled low, the status LED will start to blink rapidly until the on-board debugger
            detects the new situation and switches the target voltage regulator back on.
        Programming, debugging, and data streaming is still possible with an external power
            supply – the debugger and signal level shifters will be powered from the USB cable. Both
            regulators, the debugger, and the level shifters are powered down when the USB cable is
            removed.
        Info: In
            addition to the power consumed by the PIC18F57Q43 and its
            peripherals, approximately 100 µA will be drawn from any external power source to power
            the on-board level shifters and voltage monitor circuitry when a USB cable is plugged in
            the DEBUG connector on the board. When a USB cable is not plugged in, some current is
            used to supply the level shifters voltage pins, which have a worst-case current
            consumption of approximately 5 µA. Typical values may be as low as 100 nA.