3.1.3.8 Read Device/Revision ID
The Read Device ID command (0x24) and the Read Revision ID command
(0x28) will return the 16-bit Device ID and 16-bit Revision ID
words, respectively, when the ICSP interface has been disabled using the
ICSPDIS configuration bit. These 16-bit words are embedded
in the 24-bit data payload, as shown in Figure 1 and in Figure 2, respectively.
If the Programming and Debugging Interface Disable (PDID) feature is not being used
(i.e., ICSPDIS = 1), or if the ICSP interface has temporarily
been re-enabled using firmware stored in the device boot block (refer to the
"Software ICSP Enable" section of the "Enhanced Code Protection"
chapter in the device data sheet for more information), this command will always return
a constant value of 0xA5A5. This method can be used during production
programming to identify if the ICSPDIS feature has been enabled correctly.