Introduction

The Microchip CryptoAuth Trust Manager is a variant of the CryptoAuth Trust Platform Board and part of the CryptoAuthentication™ evaluation kits portfolio.

The CryptoAuth Trust Manager kit was developed to work with the Kudelski IoT SaaS to offer PKI service and in-field provisioning. The board contains the ECC608-TMNGTLS Trust Manager device, which is a pre-provisioned variant of the ECC608. The ECC608-TMNGTLS device will work in combination with the keySTREAM™ Software-as-a-Service (SaaS) powered by Kudelski IoT. The device comes pre-provisioned with a birth certificate and associated private key. When deployed in the marketplace, the IoT device containing the ECC608-TMNGTLS will connect to the keySTREAM SaaS, which will give ownership of the IoT device to the intended owner by provisioning the device “in-field” with its custom PKI, symmetric keys and/or data.

This user guide provides a physical overview of the connections, components and features associated with the CryptoAuth Trust Manager development kit.

Figure . CryptoAuth Trust Manager