3 mikroBUS and Click Add-On Boards

The mikroBUS connector has emerged as a de facto industry-standard add-on board form factor. The CryptoAuth Trust Manager board has a single mikroBUS host connector. Having this capability dramatically expands the usefulness of this board for developing and prototyping new applications. All of the boards listed below were developed by Microchip or MikroElektronika with support from Microchip.

Table 3-1. mikroBUS™ Add-On Boards
Board NameDevices SupportedManufacturerDescription

ATECC608_TRUST

DT100104(2)

ATECC608B-TNGTLS

ATECC608B-TFLXTLS

ATECC608B-MAHDA

MicrochipThe ECC608-TMNGTLS Trust board provides additional sample units for doing development work. This board was developed as an alternative to using socketed boards. Each of the devices can be individually selected using the on-board DIP switches.

TA010 CRYPTOAUTO

EV74C12A

TA010

MicrochipThe TA010 CryptoAuto board

ECC204 CRYPTOAUTH

EV92R58A

ECC204

MicrochipThe ECC204 CryptoAuth board

TA100-24

EV39Y17A

TA100

MicrochipThe TA100-24 socket board for the 24 VQFN device

TA100-08

AC164167

TA100 and TA010

MicrochipThe TA100-08 was developed as an 8-pin SOIC socketed solution for configuring and provisioning CryptoAuto™ devices. These devices may be used to mount to early prototype or production boards.

Contact 3

EV27Y72A

RBH parts

MicrochipThe 3 Lead Contact board was developed as an 3 Lead RBH socketed solution for configuring and provisioning CryptoAuth™ devices. These devices may be used to mount to early prototype or production boards.

VSFN socket

EV98D91A

SHA106MicrochipThe uVSFN 2 Lead Contact board was developed as a 2 Lead uVSFN socketed solution for configuring and provisioning the SHA106. These devices may be used to mount to early prototype or production boards.
Secure UDFN ClickAll Microchip CryptoAuthentication devicesMikroElektronikaThe secure UDFN Click board™ was developed as an 8-pin UDFN socketed solution for configuring and provisioning CryptoAuthentication™ devices. These devices may be used to mount to early prototype or production boards.
Secure SOIC ClickAll Microchip CryptoAuthentication devicesMikroElektronikaThe secure SOIC click board was developed as an 8-pin SOIC socketed solution for configuring and provisioning CryptoAuthentication devices. These devices may be used to mount to early prototype or production boards.
WiFi 7 ClickATWINC1510MikroElektronikaThis is the WiFi® module utilizing the ATWINC510. The board supports IEEE® 802.11 b/g/n protocols and communicates over the SPI interface.
Secure 4 Click(1)ATECC608AMikroElektronikaThis has a generic ATECC608A secure element with an I2C interface. This device is a previous version of the ATECC608B TrustCustom device that is mounted on the CryptoAuth Trust Manager board.
Secure Click(1)ATECC508AMikroElektronikaThis has a generic ATECC508A secure element with an I2C interface.
Secure 3 ClickATSHA204AMikroElektronikaThis has a generic ATSHA204A secure element with an I2C interface. The device has a cryptographic coprocessor with symmetric secure hardware-based key storage.
Secure 6 ClickATSHA204AMikroElektronikaThis has a generic ATSHA204A secure element with a SWI interface. The device has a cryptographic coprocessor with symmetric secure hardware-based key storage.
mikroBUS ShuttleClick expansion boardsMikroElektronikaThe mikroBUS Shuttle is a small add-on board that can be used to expand the mikroBUS to multiple mikroBUS connectors.
Shuttle ClickClick expansion boardsMikroElektronikaThe Shuttle Click is a socket expansion board that provides an elegant solution for stacking up to four Click boards.
Note:
  1. Not recommended for new designs.
  2. A previous version of the board used ATECC608A devices.