2 Hardware Installation
After installing the software successfully, connect one end of the USB cable to the FlashPro6 device programmer and the other end to the USB port of the PC. Use the wizard to install the driver, then ensure that you have properly installed the FlashPro software prior to installing the hardware.
Note:
FlashPro6 does not use pin 4 and pin 7 of the JTAG connector, which is different from FlashPro4 and FlashPro5. For FlashPro6, pin 4 and pin 7 of the JTAG header must not be connected.