1.54 CLASSB_Init
Function
static CLASSB_INIT_STATUS CLASSB_Init(void);Summary
This function is executed on every device reset. This shall be called right after the reset, before any other initialization is performed.
Description
This function performs the following,
a. It initializes the global variables used by the Class B library.
b. Checks the reset cause and decides next course of action.
c. If the reset is not caused by the Class B library, it tests the reserved SRAM area, clears all self-test results and performs a WDT test.
Precondition
None.
Parameters
None.
Returns
CLASSB_SST_DONE if all SSTs are successfully executed. CLASSB_SST_NOT_DONE if SSTs are yet to be executed.
Example
CLASSB_INIT_STATUS init_status = CLASSB_Init();
Remarks
None.