7.1.7 Test the Image

Insert the SD card into the board and press Reset. The Secure Boot Mode prompt should appear on the console, and then at91bootstrap and U-Boot will start running. At this point, all testing has been performed using one of the MPU's OTPC emulation modes.

Note: If power is removed from the device, all Secure mode settings will be reset.