27.2.5 ADC Conversion Procedure
This is an example procedure for using the ADC to perform an Analog-to-Digital Conversion:
- Configure Port:
- Disable the pin output driver (Refer to the TRISx register)
- Configure the pin as analog (Refer to the ANSELx register)
- Configure the ADC module:
- Select the ADC conversion clock
- Configure the voltage reference
- Select the ADC input channel
- Configure result format
- Turn on the ADC module
- Configure ADC interrupt (optional):
- Clear ADC interrupt flag
- Enable ADC interrupt
- Enable the peripheral interrupt (PEIE bit)
- Enable global interrupt (GIE bit)(1)
- Wait the required acquisition time(2).
- Start conversion by setting the GO bit.
- Wait for ADC conversion to complete by
one of the following:
- Polling the GO bit
- Waiting for the ADC interrupt (if interrupt is enabled)
- Read ADC Result.
- Clear the ADC interrupt flag (if interrupt is enabled).
Note:
- With global interrupts disabled (GIE
=
0), the device will wake from Sleep but will not enter an Interrupt Service Routine. - Refer to the “ADC Acquisition Requirements” section for more details.
ADC Conversion (assembly)
; This code block configures the ADC for polling,
; VDD and VSS references,
; ADCRC oscillator, and AN0 input.
; Conversion start & polling for completion are included.
BANKSEL TRISA
BSF TRISA,0 ; Set RA0 to input
BANKSEL ANSEL
BSF ANSEL,0 ; Set RA0 to analog
BANKSEL ADCON0
CLRF ADCON0
CLRF ADCON1
CLRF ADACT ; Auto-conversion disabled
BSF ADCON0,0 ; CHS = RA0, ADC ON
MOVLW B’11110000’ ; FM = Right-justified, CS = ADCRC, PREF = VDD
MOVWF ADCON1
CALL SampleTime ; Acquisition delay
BANKSEL ADCON0
BSF ADCON0,GO ; Start conversion
BTFSC ADCON0,GO ; Is conversion done?
GOTO $-1 ; No, test again
BANKSEL ADRESH
MOVF ADRESH,W ; Read upper byte
MOVWF RESULTHI ; Store in GPR space
MOVF ADRESL,W ; Read lower byte
MOVWF RESULTLO ; Store in GPR space
ADC Conversion (C)
/*This code block configures the ADC
for polling, VDD and VSS references,
ADCRC oscillator and AN0 input.
Conversion start & polling for completion
are included.
*/
void main() {
//System Initialize
initializeSystem();
// Configure Port
TRISAbits.TRISA0 = 1; // Set RA0 to input
ANSELAbits.ANSELA0 = 1; // Set RA0 to analog
// Configure ADC
ADCON1bits.CS = 1; // ADCRC Clock
ADCON1bits.PREF = ‘b11; // VDD
ADCON0bits.CHS = ‘b000000; // RA0
ADCON1bits.FM = 1; // Right justify
ADCON0bits.ON = 1; // Turn ADC On
while (1) {
ADCON0bits.GO = 1; // Start conversion
while (ADCON0bits.GO); // Wait for conversion done
resultHigh = ADRESH; // Read result
resultLow = ADRESL; // Read result
}
}