4 RF Spectrum
The following figure shows the RF spectrum for the ATA8352 module for the composite signal (with low and high modulation switched on).
Note: The RF filter is not used in the
current version of the module, that is, the spectrum shown is the RF output signal of
the device with the default settings, fTX at 6.52 GHz.