6 Appendix 4: Running the TCL Script
(Ask a Question)TCL scripts are provided in the design files folder under directory
TCL_Scripts. If required, the design flow can be reproduced from Design
Implementation window till generation of job file.
To run the TCL, perform the following steps:
- Launch the Libero software
- Select
- Click Browse and
select
script.tclfrom the downloadedTCL_Scriptsdirectory. - Click Run.
After successful execution of TCL script, Libero project is created within
TCL_Scripts directory.
For more information about TCL scripts, see
mpf_AN4661_v2024p1_eval_df/TCL_Scripts/TCL_Script_readme.txt.
For more details on TCL commands, see Tcl Commands Reference Guide . Contact Technical Support for any queries encountered while running the TCL script.