3.5.2 THD
Due to the limit of the code size, THD is not provided directly by the metrology firmware, but you can get them by the following formulas:
Where:
- I1 is the amplitude of fundamental harmonic current
- V1 is the amplitude of fundamental harmonic voltage
- Irms is the all harmonics current RMS value
- Vrms is the all harmonics voltage RMS value
- I1 rms is the fundamental harmonic current RMS value
- V1 rms is the fundamental harmonic voltage RMS value