1 Definitions, Acronyms and Abbreviations

Table 1-1. Abbreviations and Acronyms
AbbreviationDescription
ADCAnalog-to-Digital Converter of the ATSENSE or MCP391x AFE, consisting of a PGA, a second order Delta-Sigma modulator, and followed by an integrated third order sinc3 decimation filter. A digitized conversion of an analog voltage, VADCin, is created using the following equation:

For best linearity, the product of ADC input voltage and the PGA gain must not exceed 0.5V (GPGA * VADCin ≤ 0.5V) for the ATSENSE AFE, or 0.6V (GPGA * VADCin ≤ 0.5V) for the MCP391x AFE. GPGA for all voltage channels is fixed at 1 in the case of the ATSENSE AFE.

AFEAnalog Front End
BAMS

Binary Angular Measurement System. Angles are normalized to the binary range [-1.0000, +0.9999] k, where, k may represent any convenient scale, such as 180°, or π-radians. All angles are drawn as if vectors starting to 0° (3 o’clock position) and rotating counter-clockwise for positive phase increases. Using BAMS allows for smooth rollover from ±180º to ∓180º without edge-effects.

CTCurrent Transformer
Δ/Σ ADCDelta-Sigma Analog-to-Digital Converter, an over-sampled converter with noise shaping
DSPDigital Signal Processing
GPGA

Gain selected for use in the ADC front end, GPGA.

In the case of the ATSENSE AFE the gain on the single-ended channels (used for measuring voltage) is fixed to 1, and in the case of the differential channels can be programmed to 1, 2, 4, or 8.

In the case of the MCP391x AFE, the gain options are 1, 2, 4, 8, 16, and 32.

GPGA = [1, 2, 4, 8, 16, or 32]

Kh

Watt-hour meter constant for electro-mechanical meters, defines an amount of energy indicated by one (1) pulse generated by the meter and does not usually apply to solid-state meters.

KtWatt-hour meter test constant for solid-state meters, defines an amount of energy indicated by one (1) optical pulse generated by the meter and does not usually apply to electro-mechanical meters.
MSB

Most Significant Bit, the left-most bit of a binary number.

N

The number of samples in any one measurement interval. This number may vary for each measurement interval.

OSROver Sample Rate
Qformat

To prevent ambiguity, this document uses the following definition of Qformat numbers, being a fixed-point number format representing both integer and fractional numbers, and may be unsigned (uQm.n) or signed (sQm.n).

Unsigned Qformat numbers: An (m+n)-bit unsigned number is designated uQm.n. It occupies (m+n) bits and is stored as an unsigned fixed-point binary number. An unsigned uQm.n number may represent numbers in the range: [0, +(2m - 2-n)].

Signed Qformat numbers: An (m+n+1)-bit signed number is designated sQm.n. It occupies (m+n+1) bits and is stored as a signed fixed-point binary number, where the MSB is used as a sign bit. A signed sQm.n number may represent numbers in the range: [-(2m), +(2m - 2-n)]].

For example, an 8-bit sQ4.3 format number has one (1) sign bit, four (4) bits to the left of the binary point and three (3) bits to the right of the binary point and may be used to represent numbers in the range: [-(24), +(24 - 2-3)]] = [-16, +15.875].

To convert a sQm.n format number to a decimal equivalent, divide the equivalent twos-complement binary number by 2n. For example: an 8-bit signed sQ2.5 number: [0b0100 0001] = 65/(25) = 2.03125, an 8-bit [0b1100 0001] = -63/(25) = -1.96875.

To convert a decimal number into a sQm.n format number, multiply by 2n and convert to a signed two’s-complement (m+n+1)-bit number. For example: -7.33 => sQ3.4: (-7.33)*(24) = -117 => -[0b0111 0101] => [0b1000 1011].

Example-1: sQ1.14

A signed 16-bit number, having 1 sign bit, 1 integer bit to the left of the binary point, and 14 mantissa bits to the right of the binary point that can represent numbers in the range: [-2.0, +1.999938965].

Example-2: uQ2.14

An unsigned 16-bit number, having no sign bit, 2 integer bits to the left of the binary point and 14 mantissa bits to the right of the binary point that can represent numbers in the range: [0, +3.999938965].

PGA

Programmable Gain Amplifier: Some of the channels have an internal, selectable, programmable gain amplifier that can provide an additional analog gain equal to GPGA.

GPGA = [1, 2, 4, 8, 16 or 32]

VP, VP-M

Voltage potential: VP is the voltage measured from node P to an implied neutral reference voltage.

VP-M is the voltage measured from node P to node M, where a positive voltage is indicative of a voltage rise from node M to node P.

All phase diagrams are drawn as if mathematical vectors starting at 0° (3 o’clock) and rotating counter-clockwise for positive phase increases, with 90° being at 12 o’clock, 180° at 9 o’clock and 270° at 6 o’clock.