9.1 Debugger Selection and Switching
Use the Project Properties dialog to select or switch debuggers for a project. To switch you must have more than one debugger connected to your computer. MPLAB X IDE will differentiate between the debuggers by displaying different serial numbers.
To select or change the debugger used for a project:
- Open the Project Properties dialog by doing one of the following:
- Click on the project name in
the Projects window and select File > Project
Properties.
or
- Right click on the project name in the Projects window and select Properties.
- Click on the project name in
the Projects window and select File > Project
Properties.
- Under Categories on the left side, expand “Conf:[default]” to show your debugger, for example PICkit™ 4 or Snap, etc.
- Under Hardware Tools, find your debugger and click on a serial number (SN) to select a debugger for use in the project, then click Apply.