2 Kit Overview
The WILCS02 M.2 Wi-Fi® Module Card is an M.2 board containing the low-power WILCS02UE Module. The signals required for the control interface are connected to the M.2 Key-E connector of the M.2 board for connectivity, security and ease-of-use requirements.
Note: The following sample silkscreen is a
WIxCS02 M.2
Wi-Fi® Module Card, which includes the WILCS02 Link controller module
with Link Controller Firmware.