4.4 Get Device Support for MPLAB® X IDE
MPLAB X: Use the MPLAB Pack Manager, found under Tools→Packs, to add support for new devices in MPLAB X.
For the PIC18-Q24 Family, update to the latest version by performing the following steps:
- Click Check for Updates.
- For the PIC18F Family, select the latest available version of PIC18F-Q Series Device Support.
- Click Install.
For offline installers, go to packs.download.microchip.com. Double click on the installer file and follow the instructions to install a package. Any open MPLAB X window must be closed for the installation to take effect.