2.1.3 Inverse Park Transformation

The Inverse Park Transformation transforms electrical signals from the rotating two-axis orthogonal reference frame (dq) to the two-axis orthogonal stationary reference frame (ɑβ) as shown in the following figure.

Figure 2-4. Inverse Park Transformation

The transform is expressed by the following equations:

u α =   U d cos ( θ e ) ⁢ −   U q sin ( θ e )
u β ⁢ =   U d sin ( θ e ) ⁢ +   U q cos ( θ e )

Where:

Ud and Uq are voltages in the two-axis orthogonal dq rotating reference frame, and Uα and Uβ are voltages in the two-axis orthogonal αβ reference frame.