2.1.4 Inverse Clarke Transformation

The Inverse Clarke Transformation transforms electrical signals from the stationary two axis orthogonal reference frame (αβ) to the three axis reference frame (abc) as shown in the following figure.

Figure 2-5. Inverse Clarke Transformation

The transform is expressed by the following equations:

U a ⁢ =   U α
U b ⁢ =   −   1 2 U α +   3 2 ⁢ U β
U c ⁢ =   −   1 2 U α −   3 2 ⁢ U β

Where:

Uα and Uβ are the two-phase orthogonal voltages in the αβ reference frame, Ua, Ub, and Uc are the three-phase voltages in the abc reference frame.