3.5.3 Push Button Switches
The SAM9X75-Curiosity board features four push buttons:
- One general purpose button (SW1) connected to GPIO PC09. This is free for user application usage.
- One wake-up button (SW2) connected to WKUP0. When pressed, the processor exits from Shutdown state.
- One board reset button (SW3). When pressed, the processor is reset.
- One Start push button (SW4) connected to the MCP16502 pin. When pressed, the PMIC start-up sequence is initiated if the buck converters are off.
The following figure shows the push buttons implementation.
The following table shows the user push button signal description.
| PIO | Signal Name | Signal Description |
|---|---|---|
| PC09 | USER_BUTTON | General purpose input |