6.1.1 AT24C04C Device Addressing
Accessing the device requires an 8-bit device address byte following a Start condition to enable the device for a read or write operation. Since multiple client devices can reside on the serial bus, each client device must have its own unique address so the host can access each device independently.
The Most Significant four bits of the device address byte is referred to as
the device type identifier. The device type identifier ‘1010’ (Ah) is
required in bits 7 through 4 of the device address byte (see Table 6‑1).
Following the 4-bit device type identifier are the hardware client address bits, A2 and A1.
These bits can be used to expand the address space by allowing up to four Serial EEPROM
devices on the same bus. The A2 and A1 values must correlate with the voltage level on the
corresponding hardwired device address input pins A1 and A2. The A1 and A2 pins use an
internal proprietary circuit that automatically biases the pin to a logic
‘0’ state if the pin is allowed to float. In order to operate in a wide
variety of application environments, the pull‑down mechanism is intentionally designed to
be somewhat strong. Once these pins are biased above the CMOS input buffer’s trip point
(~0.5 x VCC), the pull-down mechanism disengages. Connecting the A1 and A2 pins
to a known state is recommended whenever possible.
When using the SOT23 package, the A1 and A2 pins are not accessible and are
left floating. The previously mentioned automatic pull‑down circuit will set these pins to
a logic ‘0’ state. As a result, to properly communicate with the device in
the SOT23 package, the A2 and A1 software bits must always be set to logic
‘0’ for any operation.
Following the A2 and A1 hardware client address bits is bit A8 (bit 1 of the device address byte), which is the Most Significant bit of the memory array word address. Refer to Table 6-1 to review the bit position.
The eighth bit (bit 0) of the device address byte is the Read/Write Select bit. A read operation is initiated if this bit is high and a write operation is initiated if this bit is low.
Upon the successful comparison of the device address byte, the AT24C04C will return an ACK. If a valid comparison is not made, the device will NACK.
| Package | Device Type Identifier | Hardware Client Address Bits | Most Significant Bit of the Word Address | R/W Select | ||||
|---|---|---|---|---|---|---|---|---|
| Bit 7 | Bit 6 | Bit 5 | Bit 4 | Bit 3 | Bit 2 | Bit 1 | Bit 0 | |
| SOIC, TSSOP, UDFN, PDIP, VFBGA | 1 | 0 | 1 | 0 | A2 | A1 | A8 | R/W |
| SOT23 | 1 | 0 | 1 | 0 | 0 | 0 | A8 | R/W |
For all operations except the current address read, a word address byte must be transmitted to the device immediately following the device address byte. The word address byte consists of the remaining eight bits of the 9-bit memory array word address, and is used to specify which byte location in the EEPROM to start reading or writing. Refer to Table 6-2 to review these bit positions.
| Bit 7 | Bit 6 | Bit 5 | Bit 4 | Bit 3 | Bit 2 | Bit 1 | Bit 0 |
|---|---|---|---|---|---|---|---|
| A7 | A6 | A5 | A4 | A3 | A2 | A1 | A0 |