36.3.2 Transmit Only Mode
When BMODE = 1, data transfers will occur whenever the transmit FIFO is
not empty. Data will be transmitted as soon as the SPIxTXB register is written to,
matching the functionality of the SPI (MSSP) modules on previous 8-bit devices. The
SPIxTCNT will decrement with each transfer. However, when SPIxTCNT is zero, the next
transfer is not inhibited and the corresponding SPIxTCNT decrement will cause the count
to roll over to the maximum value. Any data received in this mode is not stored in the
receive FIFO. The following figure shows an example of sending a command and then
sending a byte of data using this mode.
1, RXR = 0When BMODE = 0, the transfer counter (SPIxTCNT) must also be
written to before transfers will occur, and transfers will cease when the transfer
counter reaches ‘0’.
For example, if SPIxTXB is written twice and then SPIxTCNTL is written with
‘3’, the transfer will start with the SPIxTCNTL write. The two
bytes in the TXFIFO will be sent after which the transfer will suspend until the third
and last byte is written to SPIxTXB.