47.1 Standard Instruction Set
The standard PIC18 instruction set adds many enhancements to the previous PIC® MCU instruction sets while maintaining an easy migration from these PIC MCU instruction sets. Most instructions are a single program memory word (16 bits), but there are a few instructions that require two- or three-program memory locations.
Each single-word instruction is a 16-bit word divided into an opcode that specifies the instruction type and one or more operands, which further specifies the operation of the instruction.
The instruction set is highly orthogonal and is grouped into four basic categories:
- Byte-oriented operations
- Bit-oriented operations
- Literal operations
- Control operations
The PIC18 instruction set summary in Table 47-2 lists byte-oriented, bit-oriented, literal and control operations. Table 47-1 shows the opcode field descriptions.
Most byte-oriented instructions have three operands:
- The file register (specified by ‘f’)
- The destination of the result (specified by ‘d’)
- The accessed memory (specified by ‘a’)
The file register designator ‘f’ specifies which file register is to be used by the instruction. The destination designator ‘d’ specifies where the result of the operation is to be placed. If ‘d’ is zero, the result is placed in the WREG register. If ‘d’ is one, the result is placed in the file register specified in the instruction.
All bit-oriented instructions have three operands:
- The file register (specified by ‘f’)
- The bit in the file register (specified by ‘b’)
- The accessed memory (specified by ‘a’)
The bit field designator ‘b’ selects the number of the bit affected by the operation, while the file register designator ‘f’ represents the number of the file in which the bit is located.
The literal instructions may use some of the following operands:
- A literal value to be loaded into a file register (specified by ‘k’)
- The desired FSR register to load the literal value into (specified by ‘f’)
- No operand required (specified by ‘—’)
The control instructions may use some of the following operands:
- A program memory address (specified by ‘n’)
- The mode of the
CALLorRETURNinstructions (specified by ‘s’) - The mode of the table read and table write instructions (specified by ‘m’)
- No operand required (specified by ‘—’)
All instructions are a single word, except for a few two- or three-word
instructions. These instructions were made two- or three-words to contain the required
information in 32 or 48 bits. In the second and third words, the four MSbs are
‘1’s. If this second or third word is executed as an instruction
(by itself), it will execute as a NOP.
All single-word instructions are executed in a single instruction cycle,
unless a conditional test is true or the Program Counter is changed as a result of the
instruction. In these cases, the execution takes two instruction cycles, with the additional
instruction cycle(s) executed as a NOP.
The two-word instructions execute in two instruction cycles and three-word instructions execute in three instruction cycles.
One instruction cycle consists of four oscillator periods. Thus, for an oscillator frequency of 4 MHz, the normal instruction execution time is 1 μs. If a conditional test is true or the Program Counter is changed as a result of an instruction, the instruction execution time is 2 μs. Two-word branch instructions (if true) take 3 μs.
Figure 47-1, Figure 47-2 and Figure 47-3
show the general formats that the instructions can have. All examples use the convention
‘nnh’ to represent a hexadecimal number.
The Instruction Set Summary, shown in Table 47-2, lists the standard instructions recognized by the Microchip MPASMTM Assembler.
The Standard Instruction Set section provides a description of each instruction.
| Field | Description |
|---|---|
a
|
RAM access bit |
ACCESS
| ACCESS = 0: RAM access bit
symbol |
BANKED
| BANKED = 1: RAM access bit
symbol |
bbb
| Bit address within an 8-bit file register (0 to 7) |
BSR
| Bank Select Register (BSR). Used to select the current RAM bank. |
d
|
Destination select bit |
dest
| Destination: either the WREG register or the specified register file location |
f
| 8-bit register file
address (00h to FFh) |
fn
| FSR Number (0 to 2) |
fs
| 12-bit register file
address (000h to FFFh) or 14-bit register file address
(0000h to 3FFFh). This is the source address. |
fd
| 12-bit register file
address (000h to FFFh) or 14-bit register file address
(0000h to 3FFFh). This is the destination address. |
zs
| 7-bit literal offset
for FSR2 to used as register file address (000h to FFFh).
This is the source address. |
zd
| 7-bit literal offset
for FSR2 to used as register file address (000h to FFFh).
This is the destination address. |
k
| Literal field, constant data or label (may be either a 6-bit, 8-bit, 12-bit or a 20-bit value) |
label
| Label name |
|
|
The mode of the TBLPTR register for the table read and table write instructions. Only used with table read and table write instructions: No change to register (such as TBLPTR with table reads and writes) Post-Increment register (such as TBLPTR with table reads and writes) Post-Decrement register (such as TBLPTR with table reads and writes) Pre-Increment register (such as TBLPTR with table reads and writes) |
n
| The relative address (two’s complement number) for relative branch instructions or the direct address for call/branch and return instructions |
PRODH
| Product of multiply high byte |
PRODL
| Product of multiply low byte |
s
|
Fast Call/Return mode select bit |
u
| Unused or unchanged |
W
| W =
0: Destination select bit symbol |
WREG
| Working register (accumulator) |
x
| Don’t care
(‘0’ or ‘1’). The assembler will generate code with x =
0. It is the recommended form of use for compatibility with all Microchip
software tools. |
TBLPTR
| 21-bit Table Pointer (points to a program memory location) |
TABLAT
| 8-bit table latch |
TOS
| Top-of-stack (TOS) |
PC
| Program Counter |
PCL
| Program Counter low byte |
PCH
| Program Counter high byte |
PCLATH
| Program Counter high byte latch |
PCLATU
| Program Counter upper byte Latch |
GIE
| Global Interrupt Enable bit |
WDT
| Watchdog Timer |
TO
| Time-Out bit |
PD
| Power-Down bit |
C, DC, Z, OV, N
| ALU Status bits: Carry, Digit Carry, Zero, Overflow, Negative |
{ }
| Optional argument |
[ ]
| Indexed address |
( )
| Contents |
< >
| Register bit field |
[expr]<n>
| Specifies bit n of the
register indicated by pointer expr |
→
| Assigned to |
∈
| In the set of |
italics
| User defined term (font is Courier) |
| Mnemonic, Operands | Description | Cycles | 16-Bit Instruction Word | Status Affected | Notes | ||||
|---|---|---|---|---|---|---|---|---|---|
| MSb | LSb | ||||||||
| BYTE-ORIENTED FILE REGISTER INSTRUCTIONS | |||||||||
| ADDWF | f, d, a | Add WREG and f | 1 | 0010 |
01da
|
ffff
|
ffff
| C, DC, Z, OV, N | 1 |
| ADDWFC | f, d, a | Add WREG and Carry bit to f | 1 |
0010
|
00da
|
ffff
|
ffff
| C, DC, Z, OV, N | 1 |
| ANDWF | f, d, a | AND WREG with f | 1 |
0001
|
01da
|
ffff
|
ffff
| Z, N | 1 |
| CLRF | f, a | Clear f | 1 |
0110
|
101a
|
ffff
|
ffff
| Z | |
| COMF | f, d, a | Complement f | 1 |
0001
|
11da
|
ffff
|
ffff
| Z, N | 1 |
| DECF | f, d, a | Decrement f | 1 |
0000
|
01da
|
ffff
|
ffff
| C, DC, Z, OV, N | 1 |
| INCF | f, d, a | Increment f | 1 |
0010
|
10da
|
ffff
|
ffff
| C, DC, Z, OV, N | 1 |
| IORWF | f, d, a | Inclusive OR WREG with f | 1 |
0001
|
00da
|
ffff
|
ffff
| Z, N | 1 |
| MOVF | f, d, a | Move f to WREG or f | 1 |
0101
|
00da
|
ffff
|
ffff
| Z, N | 1 |
| MOVFF | fs, fd | Move fs
(12-bit source) to fd (12-bit destination) | 2 |
1100
|
fsfsfsfs
|
fsfsfsfs
|
fsfsfsfs
| None | 1, 3, 4 |
1111
|
fdfdfdfd
|
fdfdfdfd
|
fdfdfdfd
| ||||||
| MOVFFL | fs, fd | Move fs (14-bit source) to fd (14-bit destination) | 3 |
0000
|
0000
|
0110
|
fsfsfsfs
| None | 1, 3 |
1111
|
fsfsfsfs
|
fsfsfsfs
|
fsfsfdfd
| ||||||
1111
|
fdfdfdfd
|
fdfdfdfd
|
fdfdfdfd
| ||||||
| MOVWF | f, a | Move WREG to f | 1 |
0110
|
111a
|
ffff
|
ffff
| None | |
| MULWF | f, a | Multiply WREG with f | 1 |
0000
|
001a
|
ffff
|
ffff
| None | 1 |
| NEGF | f, a | Negate f | 1 |
0110
|
110a
|
ffff
|
ffff
| C, DC, Z, OV, N | 1 |
| RLCF | f, d, a | Rotate Left f through Carry | 1 |
0011
|
01da
|
ffff
|
ffff
| C, Z, N | 1 |
| RLNCF | f, d, a | Rotate Left f (No Carry) | 1 |
0100
|
01da
|
ffff
|
ffff
| Z, N | 1 |
| RRCF | f, d, a | Rotate Right f through Carry | 1 |
0011
|
00da
|
ffff
|
ffff
| C, Z, N | 1 |
| RRNCF | f, d, a | Rotate Right f (No Carry) | 1 |
0100
|
00da
|
ffff
|
ffff
| Z, N | 1 |
| SETF | f, a | Set f | 1 |
0110
|
100a
|
ffff
|
ffff
| None | |
| SUBFWB | f, d, a | Subtract f from WREG with Borrow | 1 |
0101
|
01da
|
ffff
|
ffff
| C, DC, Z, OV, N | 1 |
| SUBWF | f, d, a | Subtract WREG from f | 1 |
0101
|
11da
|
ffff
|
ffff
| C, DC, Z, OV, N | 1 |
| SUBWFB | f, d, a | Subtract WREG from f with Borrow | 1 |
0101
|
10da
|
ffff
|
ffff
| C, DC, Z, OV, N | 1 |
| SWAPF | f, d, a | Swap nibbles in f | 1 |
0011
|
10da
|
ffff
|
ffff
| None | 1 |
| XORWF | f, d, a | Exclusive OR WREG with f | 1 |
0001
|
10da
|
ffff
|
ffff
| Z, N | 1 |
| BYTE-ORIENTED SKIP INSTRUCTIONS | |||||||||
| CPFSEQ | f, a | Compare f with WREG, skip if = | 1 – 4 |
0110
|
001a
|
ffff
|
ffff
| None | 1, 2 |
| CPFSGT | f, a | Compare f with WREG, skip if > | 1 – 4 |
0110
|
010a
|
ffff
|
ffff
| None | 1, 2 |
| CPFSLT | f, a | Compare f with WREG, skip if < | 1 – 4 |
0110
|
000a
|
ffff
|
ffff
| None | 1, 2 |
| DECFSZ | f, d, a | Decrement f, Skip if 0 | 1 – 4 |
0010
|
11da
|
ffff
|
ffff
| None | 1, 2 |
| DCFSNZ | f, d, a | Decrement f, Skip if Not 0 | 1 – 4 |
0100
|
11da
|
ffff
|
ffff
| None | 1, 2 |
| INCFSZ | f, d, a | Increment f, Skip if 0 | 1 – 4 |
0011
|
11da
|
ffff
|
ffff
| None | 1, 2 |
| INFSNZ | f, d, a | Increment f, Skip if Not 0 | 1 – 4 |
0100
|
10da
|
ffff
|
ffff
| None | 1, 2 |
| TSTFSZ | f, a | Test f, skip if 0 | 1 – 4 |
0110
|
011a
|
ffff
|
ffff
| None | 1, 2 |
| BIT-ORIENTED FILE REGISTER INSTRUCTIONS | |||||||||
| BCF | f, b, a | Bit Clear f | 1 |
1001
|
bbba
|
ffff
|
ffff
| None | 1 |
| BSF | f, b, a | Bit Set f | 1 |
1000
|
bbba
|
ffff
|
ffff
| None | 1 |
| BTG | f, b, a | Bit Toggle f | 1 |
0111
|
bbba
|
ffff
|
ffff
| None | 1 |
| BIT-ORIENTED SKIP INSTRUCTIONS | |||||||||
| BTFSC | f, b, a | Bit Test f, Skip if Clear | 1 – 4 |
1011
|
bbba
|
ffff
|
ffff
| None | 1, 2 |
| BTFSS | f, b, a | Bit Test f, Skip if Set | 1 – 4 |
1010
|
bbba
|
ffff
|
ffff
| None | 1, 2 |
| CONTROL INSTRUCTIONS | |||||||||
| BC | n | Branch if Carry | 1 – 2 |
1110
|
0010
|
nnnn
|
nnnn
|
None | 2 |
| BN | n | Branch if Negative | 1 – 2 |
1110
|
0110
|
nnnn
|
nnnn
|
None | 2 |
| BNC | n | Branch if Not Carry | 1 – 2 |
1110
|
0011
|
nnnn
|
nnnn
|
None | 2 |
| BNN | n | Branch if Not Negative | 1 – 2 |
1110
|
0111
|
nnnn
|
nnnn
|
None | 2 |
| BNOV | n | Branch if Not Overflow | 1 – 2 |
1110
|
0101
|
nnnn
|
nnnn
|
None | 2 |
| BNZ | n | Branch if Not Zero | 1 – 2 |
1110
|
0001
|
nnnn
|
nnnn
|
None | 2 |
| BOV | n | Branch if Overflow | 1 – 2 |
1110
|
0100
|
nnnn
|
nnnn
|
None | 2 |
| BRA | n | Branch Unconditionally | 2 |
1101
|
0nnn
|
nnnn
|
nnnn
|
None | 2 |
| BZ | n | Branch if Zero | 1 – 2 |
1110
|
0000
|
nnnn
|
nnnn
|
None | 2 |
| CALL | k, s | Call subroutine | 2 |
1110
|
110s
|
kkkk
|
kkkk
|
None | 2, 3 |
1111
|
kkkk
|
kkkk
|
kkkk
| ||||||
| CALLW | — | Call subroutine using WREG | 2 |
0000
|
0000
|
0001
|
0100
| None | 2 |
| GOTO | k | Go to address | 2 |
1110
|
1111
|
kkkk
|
kkkk
| None | 3 |
1111
|
kkkk
|
kkkk
|
kkkk
| ||||||
| RCALL | n | Relative Call | 2 |
1101
|
1nnn
|
nnnn
|
nnnn
| None | 2 |
| RETFIE | s | Return from interrupt enable | 2 |
0000
|
0000
|
0001
|
000s
| INTCONx STAT bits | 2 |
| RETLW | k | Return with literal in WREG | 2 |
0000
|
1100
|
kkkk
|
kkkk
| None | 2 |
| RETURN | s | Return from Subroutine | 2 |
0000
|
0000
|
0001
|
001s
| None | 2 |
| INHERENT INSTRUCTIONS | |||||||||
| CLRWDT | — | Clear Watchdog Timer | 1 |
0000
|
0000
|
0000
|
0100
| TO, PD | |
| DAW | — | Decimal Adjust WREG | 1 |
0000
|
0000
|
0000
|
0111
| C | |
| NOP | — | No Operation | 1 |
0000
|
0000
|
0000
|
0000
| None | |
| NOP | — | No Operation | 1 |
1111
|
xxxx
|
xxxx
|
xxxx
| None | 3 |
| POP |
— | Pop top of return stack (TOS) | 1 |
0000
|
0000
|
0000
|
0110
| None | |
| PUSH | — | Push top of return stack (TOS) | 1 |
0000
|
0000
|
0000
|
0101
| None | |
| RESET | — | Software device Reset | 1 |
0000
|
0000
|
1111
|
1111
| All | |
| SLEEP | — | Go into Standby mode | 1 |
0000
|
0000
|
0000
|
0011
| TO, PD | |
| LITERAL INSTRUCTIONS | |||||||||
| ADDFSR | fn, k | Add FSR (fn) with literal (k) | 1 | 1110 | 1000 | fnfnkk | kkkk | None | |
| ADDLW | k | Add literal and WREG | 1 |
0000
|
1111
|
kkkk
|
kkkk
| C, DC, Z, OV, N | |
| ANDLW | k | AND literal with WREG | 1 |
0000
|
1011
|
kkkk
|
kkkk
| Z, N | |
| IORLW | k | Inclusive OR literal with WREG | 1 |
0000
|
1001
|
kkkk
|
kkkk
| Z, N | |
| LFSR | fn, k | Load FSR(fn) with a 14-bit literal (k) | 2 |
1110
|
1110
|
00fnfn
|
kkkk
| None | 3 |
1111
|
00kk
|
kkkk
|
kkkk
| ||||||
| MOVLB | k | Move literal to BSR<5:0> | 1 |
0000
|
0001
|
00kk
|
kkkk
| None | |
| MOVLW | k | Move literal to WREG | 1 |
0000
|
1110
|
kkkk
|
kkkk
| None | |
| MULLW | k | Multiply literal with WREG | 1 |
0000
|
1101
|
kkkk
|
kkkk
| None | |
| RETLW | k | Return with literal in WREG | 2 |
0000
|
1100
|
kkkk
|
kkkk
| None | |
| SUBFSR | fn, k | Subtract literal (k) from FSR (fn) | 1 | 1110 | 1001 | fnfnkk | kkkk | None | |
| SUBLW | k | Subtract WREG from literal | 1 |
0000
|
1000
|
kkkk
|
kkkk
| C, DC, Z, OV, N | |
|
k |
Exclusive OR literal with WREG |
1 |
0000
|
1010
|
kkkk
|
kkkk
|
Z, N | ||
| DATA MEMORY – PROGRAM MEMORY INSTRUCTIONS | |||||||||
| TBLRD* | — | Table Read | 2 |
0000
|
0000
|
0000
|
1000
| None | |
| TBLRD*+ | — | Table Read with post-increment | 2 |
0000
|
0000
|
0000
|
1001
| None | |
| TBLRD*- | — | Table Read with post-decrement | 2 |
0000
|
0000
|
0000
|
1010
| None | |
| TBLRD+* | — | Table Read with pre-increment | 2 |
0000
|
0000
|
0000
|
1011
| None | |
| TBLWT* | — | Table Write | 2 |
0000
|
0000
|
0000
|
1100
| None | |
| TBLWT*+ | — | Table Write with post-increment | 2 |
0000
|
0000
|
0000
|
1101
| None | |
| TBLWT*- | — | Table Write with post-decrement | 2 |
0000
|
0000
|
0000
|
1110
| None | |
| TBLWT+* | — | Table Write with pre-increment | 2 |
0000
|
0000
|
0000
|
1111
|
None | |
|
Note:
| |||||||||