5.4.3 Probe
The Target Adapter is pictured below. The 20-wire flex-cable connects the Target Adapter to the Atmel AVR JTAGICE mkII. The Target Adapter has two 10-pin connectors that have identical pin-out, and signals. Use the one that best fits the target board. Only one of the connectors should be connected at any given time.


For further information on how to connect the probe to the target application, see section Connecting the JTAGICE mkII.