1.2.1 How the I2C Bootloader Library Works
The I2C Bootloader firmware communicates with the embedded host device by using a predefined communication protocol.
The I2C Bootloader works in two different modes:
Basic Mode
-
This mode is supported for all the devices
-
Resides from:
- The starting location of the Flash memory region for Cortex-M based MCUs
-
The Bootloader performs Flash erase/program/verify operations with the binary sent from host while in the Firmware Upgrade mode
- The binary sent is only of the application to be programmed
- Bootloader always performs Flash operation from the address for (bootloader or application) binary sent from host
- The application can use the entire Flash memory region starting from the end of bootloader space
-
Jumps to the application once verification is completed
Fail Safe Update Mode
-
This mode is supported for the devices which have a Dual Bank Flash memory
-
Resides from the starting location of the Flash memory region of both the banks on Cortex-M based MCUs
-
The Bootloader performs Flash erase/program/verify operations with the binary sent from host while in the Firmware Upgrade mode
-
Bootloader can perform Flash operation in either of the banks based on the address sent by the host application
-
The application can use only the Flash memory region of one bank.
-
-
Performs a bank swap and reset to run the application programmed in opposite bank once verification is completed or a normal reset to run the application in current bank based on command sent from host