1.6.1 How the USB Device HID Bootloader Library Works

The USB Device HID Bootloader firmware communicates with the Unified Host application running on Host PC by using a predefined communication protocol.

The USB Device HID Bootloader works in two different modes:

Basic Mode

  • This mode is supported for all the devices

  • Resides from:

    • The starting location of the Flash memory region for Cortex-M based MCUs

    • The starting location of the Boot Flash memory region or Program Flash memory region for MIPS based MCUs devices

  • The Bootloader performs Flash erase/program/verify operations with the application hex sent from host PC using the Unified Bootloader Host Application while in the Firmware Upgrade mode

    • Bootloader always performs Flash operation from the address received via hex record

    • The application can use the entire Flash memory region starting from the end of bootloader space

  • Jumps to the application once programming is completed

Live Update Mode

  • This mode is supported for the devices which have a Dual Bank Flash memory

  • Resides from:

    • The starting location of the Flash memory region of both the banks on Cortex-M based MCUs along with application code

    • The starting location of the Program Flash memory region of both the banks for MIPS based MCUs devices along with application code

  • The Bootloader task performs Flash erase/program/verify operations with the application hex sent from host PC using the Unified Bootloader Host Application in the Inactive bank

  • Performs a bank swap and reset to run the application programmed in inactive bank on application task request