1.3.3 SPI Bootloader Configurations
Bootloader Specific User Configurations
-
Bootloader Peripheral Used:
- Specifies the communication peripheral used by bootloader to receive the application
- The name of the peripheral will vary from device to device
-
Bootloader NVM Memory Used:
- Specifies the memory peripheral used by bootloader to perform Flash operations
- The name of the peripheral will vary from device to device
-
Bootloader Size (Bytes):
- Specifies the maximum size of Flash required by the bootloader
- This size is calculated based on Bootloader type and Memory used
- This size will vary from device to device and should always be aligned to device erase unit size
-
Enable Bootloader Trigger From Firmware:
-
This Option can be used to Force Trigger bootloader from application firmware after a soft reset. It does so by reserving the specified number of bytes in SRAM from the start of the RAM. The reserved memory is updated by the application with a pre-defined pattern. The bootloader firmware in the bootloader_Trigger() routine, can check the reserved memory for the pre-defined pattern and enter Bootloader mode if the pattern matches.
-
Number Of Bytes To Reserve From Start Of RAM:
- Specifies the number of bytes to reserve for the trigger pattern in RAM. This option adds the provided offset to RAM Start address in bootloader linker script.
- Application firmware can store some pattern in the reserved bytes region from RAM start for bootloader to check at reset in bootloader_Trigger() function
-
-
Enable Fuse Programming:
- Enables fuse programming capability in the bootloader
-
Enable watchdog Refresh If Enabled Through Fuse:
- Bootloader firmware refreshes the watchdog if it is enabled through fuse
-
Use Dual Bank For Safe Flash Update:
- Used to configure bootloader to use Dual banks of device to upload the application
- This option is visible only for devices supporting Dual Flash banks
Bootloader System Configurations
- Application Start Address (Hex):
- Start address of the application which will programmed by bootloader
- This value is filled by bootloader when its loaded which is equal to the bootloader size. It can be modified as per user need.
- This value will be used by bootloader to Jump to application at device reset