1.9.1 How the OTA Bootloader Library Works
OTA Bootloader - Dual Bank (For MCUs)
-
This is a OTA bootloader which resides from:
-
The starting location of the Flash memory region for SAM devices
-
The starting location of the Boot Flash memory region for PIC32M devices
- Uses a Custom linker script btl.ld to place it in Boot Flash memory
-
-
Performs Below Operation:
-
Read the control block stored in the last sector of dual bank memory
-
Checks if blockUpdated field is set to 1, then it will update the control block
- SAM devices: If blockUpdated field is set to 0 then it jumps to application space to run the OTA application
- PIC32M devices: If blockUpdated field is set to 0 then map Program Flash Bank with higher serial number to the lower region and then it jumps to Step 4
-
Set blockUpdated field to 0 and then update the control block in the dual bank Flash memory. And perform the following operation.
- SAM devices: Swap bank and trigger reset
- PIC32M devices: Trigger reset
-
Run OTA application as below:
-
Calls the SYS_Deinitialize() function which releases the resources used. This Function is device specific and has to be implemented based on application requirement.
-
Jumps to application space to run the OTA application
-
-
OTA Bootloader - External Memory (For MCUs)
-
This is a OTA bootloader which resides from:
-
The starting location of the Flash memory region for SAM devices
-
The starting location of the Boot Flash memory region for PIC32M devices
- Uses a Custom linker script btl.ld to place it in Boot Flash memory
-
-
Performs Below Operation:
-
Read the control block stored in the last sector of external memory
-
Checks if blockUpdated field is set to 1, then it will update the application binary
- If blockUpdated field is set to 0 then it jumps to application space to run the OTA application
-
If application update is required then it
- Reads the OTA application binary stored from loadAddress in the external memory
- Programs the read binary to programAddress in the Internal Flash
-
Once programming is done it generates a CRC32 value over programmed space and verifies it against the CRC32 stored in external memory control block
-
If verification is successful then set blockUpdated field to 0 and then update the control block in the external memory and trigger reset
-
Run OTA application as below:
-
Calls the SYS_Deinitialize() function which releases the resources used. This Function is device specific and has to be implemented based on application requirement.
-
Jumps to application space to run the OTA application
-
-
MPU OTA Bootloader and Applications Block Diagram
OTA Bootloader
-
This is a bootloader application which resides from:
-
OTA Bootloader stored into SD/NAND/Serial Flash memory
-
OTA Bootloader executes from DDR memory. AT91Bootstrap loads OTA bootloader from SD/NAND/Serial Flash memory to DDR memory and executes it.
-
Then OTA Bootloader loads OTA application image from SD/NAND/Serial Flash memory to DDR memory and executes it
-
Performs Below Operation:
-
Read the metadata (image size) stored in the external memory.
-
Reads the OTA application binary stored from the external memory and Programs the binary to the DDR memory.
-
Run OTA application as below:
- Calls the SYS_Deinitialize() function which releases the resources used. This Function is device specific and has to be implemented based on application requirement.
-
Jumps to application space to run the OTA application
OTA Application
-
This is a OTA application which resides from:
- OTA application stored into SD/NAND/Serial Flash memory
-
It blinks an LED and provides console output
-
It calls the OTA_SERVICE_Tasks() function which receives the binary over OTA to be programmed into the external memory
-
Once the binary is received and programmed into the external memory, it generates a CRC32 value over programmed external memory space and verifies it against the received CRC32
-
If verification is successful then it updates the metadata (image size) and trigger reset to run new application binary through OTA bootloader
Bootloader Control Block (Metadata)
/* Per app image info to store in this structure for bootloader/OTA service * Note: The order of the members should not be changed */ typedef struct __attribute__((packed)) { unsigned int status : 3; unsigned int signaturePresent : 1; unsigned int filenamePresent : 1; unsigned int imageEncrypted : 1; unsigned int reserved : 2; unsigned int imageType : 4; unsigned int imageStorage : 4; unsigned int versionNum : 4; unsigned int format : 4; unsigned int signatureType : 8; uint32_t programAddress; uint32_t jumpAddress; uint32_t loadAddress; uint8_t signature[8]; uint32_t imageSize; } APP_IMAGE_INFO;
Dual Bank (for Cortex-M based MCU)
/* Control block (Metadata) structure for bootloader/OTA service
* Note: The order of the members should not be changed
*/
typedef struct
{
unsigned int versionNum : 4;
unsigned int ActiveImageNum : 4;
unsigned int blockUpdated : 1;
unsigned int reserved : 23;
APP_IMAGE_INFO appImageInfo[1];
} OTA_CONTROL_BLOCK;
Dual Bank (for MIPS based MCU)
/* Control block (Metadata) structure for bootloader/OTA service
* Note: The order of the members should not be changed
*/
typedef struct
{
uint32_t serialNum;
unsigned int versionNum : 4;
unsigned int ActiveImageNum : 4;
unsigned int blockUpdated : 1;
unsigned int reserved : 23;
APP_IMAGE_INFO appImageInfo[1];
} OTA_CONTROL_BLOCK;
External Memory
/* Control block (Metadata) structure for bootloader/OTA service
* Note: The order of the members should not be changed
*/
typedef struct
{
unsigned int versionNum : 4;
unsigned int ActiveImageNum : 4;
unsigned int blockUpdated : 1;
unsigned int reserved : 23;
APP_IMAGE_INFO appImageInfo[2];
} OTA_CONTROL_BLOCK;
- For MCUs: The above Control Block (Metadata) for application has to be stored in last page of inactive bank (or external memory) required by bootloader
- For MPUs: Per app image info is fixed with 1 value (e.g., APP_IMAGE_INFO appImageInfo;)