1.8.4 SD Card Bootloader Configurations
Bootloader Specific User Configurations
-
Bootloader Media Type:
- Change the Media Type to SDCARD
-
Bootloader NVM Memory Used:
- Specifies the memory peripheral used by bootloader to perform Flash operations
- The name of the peripheral will vary from device to device
-
Bootloader Size (Bytes):
- Specifies the maximum size of Flash required by the bootloader
- This size is calculated based on Bootloader type and Memory used
- This size will vary from device to device and should always be aligned to device erase unit size
-
Enable Bootloader Trigger From Firmware:
-
This Option can be used to Force Trigger bootloader from application firmware after a soft reset. It does so by reserving the specified number of bytes in SRAM from the start of the RAM. The reserved memory is updated by the application with a pre-defined pattern. The bootloader firmware in the bootloader_Trigger() routine, can check the reserved memory for the pre-defined pattern and enter Bootloader mode if the pattern matches.
-
Number Of Bytes To Reserve From Start Of RAM:
- This option adds the provided offset to RAM Start address in bootloader linker script
- Application firmware can store some pattern in the reserved bytes region from RAM start for bootloader to check at reset in bootloader_Trigger() function
-
-
Application Binary Image Path:
-
Application binary image file name with path. If only file name is mentioned bootloader will try to open the file from the root directory.
-
Default: image.bin
-
Can be used to specify custom paths based on requirement
- Example: dir1/dir2/app.bin
-
File System Configurations
-
Use File System Auto Mount Feature:
- Enabled by default when File System Bootloader is added
-
Media Type:
- Change the Media Type to SYS_FS_MEDIA_TYPE_SDCARD
-
Make FAT File System Read-only:
-
Enabled by default when File System Bootloader is added as there are no write operations to be done
-
Enabling this option also saves significant amount of Flash memory
-
Bootloader System Configurations
- Application Start Address (Hex):
- Start address of the application which will programmed by bootloader
- This value is filled by bootloader when its loaded which is equal to the bootloader size. It can be modified as per user need.
- This value will be used by bootloader to jump to application at device reset
Bootloader Linker Pre Processor Macros for Cortex-M Based MCUs
- Based on the configurations the above
linker pre processor macros will be generated in MPLAB X xc32-ld settings
- ROM_LENGTH specifies the size of the bootloader