2.1 MCC Generated Code
To generate this project using MPLAB Code Configurator (MCC), follow the next steps:
- Create a new MPLAB X IDE project for PIC18F47Q10.
- Open MCC from the toolbar (more
information about how to install the MCC plug-in can
be found here.
- Go to Project Resources →
System → System Module and do the following configuration:
- Oscillator Select: HFINTOSC
- HF Internal Clock: 1 MHz
- Clock Divider: 1
- In the Watchdog Timer Enable field in WWDT tab, make sure “WDT Disabled” is selected
- In the Programming tab, make sure Low-Voltage Programming Enable is checked.
- From the Device Resources window, add
ADCC, then do the following configuration:
- Enable ADC: Check
- Operating: Basic Mode
- Clock Source: FRC
- Result Alignment: Right
- Positive Reference: VDD
- Negative Reference: VSS
- Go to Pin Manager → Grid
View and select the RA0 pin as ANx input for the ADCC.
Figure 2-1. Pin Mapping - Go to the Pin Module in the Project Resources tab and set the RA0 pin as analog and as input (check to see if output is not checked).
- Press the Generate button. The generated code can now be found in the project folder.
- Add the following code to the main
function.
Add this before the main function. This is the variable that stores the value and can be read with the debugger.
uint16_t volatile adcVal;
Add this code inside the body of themain()function. This discharges the sample capacitor and adds a function that starts the conversion on the analog channel and returns the value.ADCC_DischargeSampleCapacitor(); adcVal = ADCC_GetSingleConversion(channel_ANA0); while (1) { ; }