9.7 Reference Clock Output
In addition to the CLKO output (FOSC/2), the dsPIC33CDVL256MC506 family devices can be configured to provide a reference clock output signal to a port pin. This feature is available in all oscillator configurations and allows the user to select a greater range of clock submultiples to drive external devices in the application. CLKO is enabled by the Configuration bit (OSCIOFNC) and is independent of the REFCLKO reference clock. REFCLKO is mappable to any I/O pin that has mapped output capability. The reference clock output module block diagram is shown in Figure 9-5.
This reference clock output is controlled by the REFOCONL and REFOCONH
registers. Setting the ROEN bit (REFOCONL[15]) makes the clock signal available on the
REFCLKO pin. The RODIV[14:0] bits (REFOCONH[14:0]) and ROTRIM[8:0] bits
(REFOTRIMH[15:7]) enable the selection of different clock divider options. The formula
for determining the final frequency output is shown in Equation 9-3. The ROSWEN bit (REFOCONL[9]) indicates that
the clock divider has been successfully switched. In order to switch the REFCLKO
divider, the user should ensure that this bit reads as ‘0’. Write the
updated values to the RODIV[14:0] or ROTRIM[8:0] bits, set the ROSWEN bit, and then wait
until it is cleared before assuming that the REFCLKO clock is valid.
The ROSEL[3:0] bits (REFOCONL[3:0]) determine which clock source is used for the reference clock output. The ROSLP bit (REFOCONL[11]) determines whether the reference source is available on REFCLKO when the device is in Sleep mode.
To use the reference clock output in Sleep mode, both the ROSLP bit must be set, and the clock selected by the ROSEL[3:0] bits must be enabled for operation during Sleep mode, if possible. Clearing the ROSEL[3:0] bits allows the reference output frequency to change as the system clock changes during any clock switches. The ROOUT bit enables/disables the reference clock output on the REFCLKO pin.
The ROACTIV bit (REFOCONL[8]) indicates that the module is active; it can
be cleared by disabling the module (setting ROEN to ‘0’). The user must
not change the reference clock source or adjust the divider when the ROACTIV bit indicates
that the module is active. To avoid glitches, the user should not disable the module until
the ROACTIV bit is ‘1’.