5.2 Bootstrap Operation

The supply for the MCP14H2184 High-Side is provided by the bootstrap capacitor CB (see Figure 5-2). In the half-bridge configuration, VS swings from 0V to VHV depending on the PWM input of the IC. When VS is 0V, VBS will go below VCC, and VCC will charge CB . When HO goes high, VS swings to VHV, and VBS remains at VCC minus a diode drop (DB), due to the voltage on CB . This is the supply for the high side gate driver and allows the gate driver to function with the floating well (VS ) at the high voltage.

When considering the value of the bootstrap capacitor CB , it is important that it is sized to provide enough energy to quickly drive the gate of QH . Values of 1 μF to 10 μF are recommended. The exact value depends on gate capacitance and the noise level appropriate for the application. It is key to use a low ESR capacitor that is close to the device. This will best quickly supply charge to the gate of the MOSFET.

Figure 5-2. MCP14H2184 High-side in Bootstrap Operation