9.19 timeout_example.c File Reference
Includes
- ../drivers/timeout.h
- timeout_example.h
Functions
- uint32_t
-
oneshot_handler (void)
This timeout callback handler returns 0, does not reschedule the timer, so will execute only once.
Parameters:
- none
Returns:
None
- uint32_t
-
periodic_handler (void)
This timeout callback handler continuously reschedules a periodic timer to timeout with the number of ticks it returns.
Parameters:
- none
Returns:
None
- uint32_t
-
periodic_handler_payload (void *payload)
This handler executes a repeating, periodic timer that uses a payload argument.
Parameters:
- payload
Type: void *
- any value that needs to be passed onto the handler.
Returns:
None
- uint32_t
-
counter_handler (void)
This handler executes a repeating timer that counts the ticks while an event is going on.
Parameters:
- none
Returns:
None
- void
-
Timeout_example_create_sched_oneshot (void)
Call this function to run a 1000-tick timer once. The timer will not be rescheduled in the associated callback function.
Parameters:
- none
Returns:
None
- void
-
Timeout_example_create_sched_periodic (void)
Call this function to run a 1000-tick timer continuously. The callback function reschedules the timer continuously.
Parameters:
- none
Returns:
None
- void
-
Timeout_example_create_sched_periodic_with_payload (void)
Call this function to run a 1000-tick timer 10 times, with the counter sent as a payload.
Parameters:
- none
Returns:
None
- uint32_t
-
Timeout_example_stopwatch_mode (void)
Call this function to count how many timer ticks have elapsed since the start of a timer
Parameters:
- Type: void
Returns: