Foundation Services is a collection of software components such as peripheral drivers, middleware, and software applications (examples) provided by Microchip. The framework supports the Microchip's 8- and 16- bit PIC, as well as AVR families of microcontrollers.
Video slides from introduction to What is Foundation Services.
Video demonstrating how to use Timeout drivers Periodic Timer example code snippet.
Video demonstrating how to use Timeout drivers Oneshot Timer example code snippet.
Video demonstrating how to use Timeout driver's payload example code snippet.
Video demonstrating how to use the various UART code snippets.
Video demonstrating how to use the SPI Master Loopback example code snippet.
This file contains the API to generate delays in the millisecond and microsecond ranges.
This file contains the APIs to demonstrate the Delay Driver use cases.
This file contains the API that implements the I2C simple master driver functionalities.
This file contains the API that implements the I2C simple master driver functionalities.
This file explains the basic use cases and implementation of the Real Time Counter.
This file contains the RTCounter APIs.
This file contains the APIs to demonstrate the common use cases of the RTCounter.
The driver provides basic SPI functionality supporting both Master and Slave, each with or without interrupts.
This file contains the API that implements the SPI master driver functionalities.
This file contains the API that implements the SPI master driver example functionalities.
This file recounts the basic use cases and implementation of the Timeout Driver.
This file contains the Timeout Driver APIs.
This file contains the APIs to demonstrate the common use cases of the Timeout Driver.
This file contains the UART configurations selected by the user in the UART Foundation Services MCC Interface.
This file contains the API that implements the UART Example functionalities.
Here is a list of all documented files with brief descriptions
Here is a list of all documented files with brief descriptions