2.4 PHY Sniffer

The PHY Sniffer is an application example that uses the PHY layer to monitor G3-PLC frames in the network and send them via USI serialization. The Hybrid Sniffer PC tool is also provided to interface with the board and interpret the frames. This example requires only one board and a G3-PLC network to be monitored.

The example provided offers the serial interface configured through a certain UART or USB (depending on the platform) at 230400 bps by default.

This example is located in the folder \thirdparty\g3\phy\atpl360\apps\phy_sniffer_hybrid_tool\ of the firmware package:

Table 2-5. LEDs
DescriptionBoardLED
Reception of message RFATREB215-XPRO-ALED2
PLCPL360G55Cx-EKLED1
PL460-EK—