2.1 DLMS G3-PLC Coordinator

The DLMS example for the G3-PLC coordinator implements a DLMS client that shows how the G3-PLC API along with an IPv6 stack can be used in a typical DLMS application. The coordinator performs a continuous DLMS data collection that generates data traffic in the G3-PLC network. Besides DLMS traffic, the application can be configured to generate ICMPv6 traffic sending PINGs to other nodes.

The DLMS example for the coordinator periodically asks every device registered in the network for DLMS objects. A log can be checked using the console in the UART port.

This example is located in the folder \thirdparty\g3\apps\dlms_app_coord\ of the firmware package:

Table 2-1. LEDs
DescriptionBoardIndication
Reception of message RFATREB215-XPRO-ALED2
PLCPL360G55Cx-EKLED1
PL460-EK—
Message transmittedRFATREB215-XPRO-ALED1
PLCPL360G55Cx-EKD104/D110
PL460-EKD4