1.15 MSD SD Card Example (msd_sdcard)

This application demonstrates the ability of the MPLAB Harmony USB Device Stack to support USB Mass Storage Device. The application uses SD Card as storage media.

Description

This application creates a USB MSD Device that enumerates as a Flash Drive on the USB host PC. The application allows read / write / modify / delete data from a PC host like any normal Flash drive.

Downloading and building the application

To clone or download this application from Github, go to the main page of this repository and then click Clone button to clone this repository or download as zip file. This content can also be downloaded using content manager by following these instructions.

Path of the application within the repository is usb_apps_device/apps/msd_sdcard.

Following table gives the details of project configurations, target device used, hardware and its IDE. Open the project using the respective IDE and build it.

Project Name IDE Target Device Hardware / Configuration
pic32mx470_curiosity.X MPLABX PIC32MX470F512H PIC32MX Curiosity Development Board
pic32mz_ef_curiosity_2_0.X MPLABX PIC32MZ2048EFM144 Curiosity PIC32MZ EF 2.0 Development Board
sam_9x60_ek.X MPLABX SAM9X60 SAM9X60-EK Evaluation Board
sam_9x60_curiosity.X MPLABX SAM9X60 SAM9X60 Curiosity Development Board
sam_9x60_curiosity_freertos.X MPLABX SAM9X60 SAM9X60 Curiosity Development Board
sam_9x75_eb.X MPLABX SAM9X75 SAM9X75-DDR3-EB Evaluation Board
sam_a5d2_xult.X MPLABX ATSAMA5D27C SAMA5D2 Xplained Ultra Board
sam_a5d27_som1_ek.X MPLABX ATSAMA5D27C SAMA5D27 SOM1 Kit1
sam_a5d27_wlsom1_ek1.X MPLABX ATSAMA5D27C ATSAMA5D27 WLSOM1 EK1
sam_a7g5_ek.X MPLABX SAMA7G54 SAMA7G5 EK Board
sam_e70_xult.X MPLABX ATSAME70Q21B SAME70 Xplained Ultra Board
pic32cz_ca80_curiosity_ultra.X MPLABX PIC32CZ8110CA80208 PIC32CZ CA80 Curiosity Ultra development board
pic32ck_gc01_curiosity_ultra.X MPLABX PIC32CK2051GC01144 PIC32CK GC Curiosity Ultra Development Board
pic32cx_sg41_curiosity_ultra.X MPLABX PIC32CX1025SG41128 PIC32CX SG41 Curiosity Ultra Evaluation Board
sam_a5d29_curiosity.X MPLABX ATSAMA5D29 SAMA5D29 Curiosity Development Board
sam_9x75_curiosity.X MPLABX SAM9X75D2G SAM9X75-Curiosity Development Board
sam_a7d65_curiosity.X MPLABX SAMA7D65 SAMA7D65 Curiosity Development Board

Configuring the Hardware

SAME70 Xplained Ultra Board
  • Jumper J203 must be shorted between PB08 and VBUS (positions 2 and 3).
  • Insert the micro-SD card into the micro-SD Card slot (J700).
  • Use TARGET USB J200 connector on the board to connect the USB Device to the USB Host PC.
  • LED3 indicates USB Device Configuration Set Complete event (the USB device functionality has been activated by the USB Host).
SAM9X60-EK Evaluation Board
  • Setup the SD card (Note: exFAT formatted SD Cards are not supported)

    • Download harmony MPU bootstrap loader from this location.
    • Copy the downloaded boot loader binary (boot.bin) and generated application binary (harmony.bin) into the SD card.
    • Insert the SD card into the SDMMC connector J4 on the board.
    • Reset the board by pressing the Push Button SW3.
  • Jumpers J20, J21, and J13 must be open.

  • Jumper J2 and J3 must be shorted.

  • Connect the USB Micro-B port J22 on board to the computer using a micro USB cable (to enable the debug com port).

  • Connect the USB Micro-B Connector (J7) on the board to the computer using a micro USB cable.

  • LED D1 indicates USB Device Configuration Set Complete event (The USB device functionality has been activated by the USB Host).

    Note: Reset push button on SAM9X60 EK is labeled as SW3

SAM9X60-Curiosity Board
  • Setup the SD card (Note: exFAT formatted SD Cards are not supported)
    • Download harmony MPU bootstrap loader from this location.
    • Copy the downloaded boot loader binary (boot.bin) and generated application binary (harmony.bin) into the SD card.
    • Insert the SD card into the SDMMC0 connector J3 on the board.
    • Reset the board by pressing the Push Button "RESET".
  • Jumper J4 must be shorted.
  • Connect the USB Micro-B Connector (J1) on the board to the computer using a micro USB cable.
  • LED D1 indicates USB Device Configuration Set Complete event (The USB device functionality has been activated by the USB Host).
SAM9X75-DDR3-EB Evaluation Board
  • Powered the board with an external power supply (or use the micro AB connector).

  • Setup the SD card (Note: exFAT formatted SD Cards are not supported)

    • Download harmony MPU bootstrap loader from this location.
    • Copy the downloaded boot loader binary (boot.bin) and generated application binary (harmony.bin) into the SD card.
    • Insert the SD card into the SDMMC connector (SDMMC0) on the board.
    • Reset the board by pressing the Push Button RESET, then START.
  • Connect USB to serial cable to DBGU0 (to enable debug com port).

  • Connect the USB Micro-AB Connector on the board to the computer using a micro USB cable.

  • LED near VDDCORE inscription on the board indicates USB Device Configuration Set Complete event (The USB device functionality has been activated by the USB Host).
    SAMA5D2 Xplained Ultra Board
    • Setup the SD card (Note: exFAT formatted SD Cards are not supported)
      • Download harmony MPU bootstrap loader from this location.
      • Copy the downloaded boot loader binary (boot.bin) and generated application binary (harmony.bin) into the SD card.
      • Insert the SD card into the SDMMC1 slot on the board.
      • Reset the board by pressing the Push Button BP3.
    • Short jumper JP2(DEBUG_DIS).
    • Connect the EDBG USB Micro-B port J14 on the board to the computer using a micro USB cable.
    • Use the "A5-USB-A" connector (J23 - Micro A/B connector) on the board to connect the USB device to the USB Host.
    • RGB LED turning to Green indicates USB Device Configuration Set Complete event (The USB device functionality has been activated by the USB Host).
    Curiosity PIC32MX470 Development Board
    • To run the demo, the following additional hardware is required:
    • Insert the micro-sd click board into the Mikro BUS 1 connector on the Curiosity PIC32MX470 Development Board.
    • Insert the micro-SD card into the micro-SD Card slot of the micro-sd click board.
    • USB micro-B port J12 to connect the USB device to the USB Host PC.
    • LED1 indicates USB Device Configuration Set Complete event (the USB device functionality has been activated by the USB Host).
    Curiosity PIC32MZ EF 2.0 Development Board
    • To run the demo, the following additional hardware is required:
    • Insert the micro-sd click board into the Mikro BUS 1 connector on the Curiosity PIC32MZ EF 2.0 Development Board.
    • Insert the micro-SD card into the micro-SD Card slot of the micro-sd click board.
    • Use the USB micro-B port J201 to connect the USB Device to the USB Host PC.
    • LED1 indicates USB Device Configuration Set Complete event (the USB device functionality has been activated by the USB Host).
    SAMA5D27 SOM1 Kit1
    • Setup the SD card (Note: exFAT formatted SD Cards are not supported)
      • Download harmony MPU bootstrap loader from this location.
      • Copy the downloaded boot loader binary (boot.bin) and generated application binary (harmony.bin) into the SD card.
      • Insert the SD card into the SDMMC0 slot (J12) on the board.
      • Reset the board by pressing the Push Button PB1.
    • Connect the Debug USB port (J10) on the board to the computer using a micro USB cable.
    • Connect the USB Micro-B Connector (J17) on the board to the computer using a micro USB cable.
    • RGB LED turning to Green indicates USB Device Configuration Set Complete event (The USB device functionality has been activated by the USB Host).
ATSAMA5D27-WLSOM1 Evaluation Kit
  • Setup the SD card (Note: exFAT formatted SD Cards are not supported)
    • Download harmony MPU bootstrap loader from this location.
    • Copy the downloaded boot loader binary (boot.bin) and generated application binary (harmony.bin) into the SD card.
    • Insert the SD card into the SDMMC0 Card Connector (J9) on the board.
    • Reset the board by pressing the Reset Button (SW2)
  • Connect the USB-A MicroAB connector (J10) on the board to the computer using a micro USB cable.
  • Press the "START_SOM" button to activate board start-up.
  • RGB LED turning to Green indicates USB Device Configuration Set Complete event (The USB device functionality has been activated by the USB Host

    SAMA7G5-EK Evaluation Kit
    • Powered the board with an external power supply (J1) or power supply the board by connecting J7 to the computer using a micro USB cable.
    • Setup the SD card (Note: exFAT formatted SD Cards are not supported)
      • Download harmony MPU bootstrap loader from this location.
      • Copy the downloaded boot loader binary (boot.bin) and generated application binary (harmony.bin) into the SD card.
      • Insert the SD card into the SD Card Connector (J4) on the board.
      • Reset the board by pressing the Reset Button (nRST)
    • Press the "nSTART" button to activate board start-up.
    • Connect the USB MicroAB connector (J7) to the computer using an USB cable.
    • RGB LED turning to Green indicates USB Device Configuration Set Complete event (The USB device functionality has been activated by the USB Host).
    PIC32CZ CA80 Curiosity Ultra development board
    • To run the demo, the following additional hardware is required:

      • micro-sd card
    • Insert the micro-SD card into the micro-SD Card slot J600 of the PIC32CZ CA80 Curiosity Ultra development board.

    • Use the USB micro-B port J102 to connect the USB Device to the USB Host PC.

    • LED0 indicates USB Device Configuration Set Complete event (the USB device functionality has been activated by the USB Host).

    PIC32CK GC Curiosity Ultra Development Board
    • Use the Barrel jack connector(J200) to connect an external power supply to the board.
    • To run the demo, the following additional hardware is required:

      • micro-sd card
    • Insert the micro-SD card into the micro-SD Card slot J600 of the PIC32CK Curiosity Development Board.

    • Use the USB Type-C port J202 to connect the USB Device to the USB Host PC.

    • LED0 indicates USB Device Configuration Set Complete event (the USB device functionality has been activated by the USB Host).

    PIC32CX SG41 Curiosity Ultra Evaluation Board
    • To run the demo, the following additional hardware is required:

      • micro-sd card
    • Insert the micro-SD card into the micro-SD Card slot J704 of the PIC32CX Curiosity Development Board.

    • Use the USB micro-B port J200 to connect the USB Device to the USB Host PC.

    • LED1 indicates USB Device Configuration Set Complete event (the USB device functionality has been activated by the USB Host).

    SAMA5D29 Curiosity Development Board

    • Setup the SD card (Note: exFAT formatted SD Cards are not supported)
      • Download harmony MPU bootstrap loader from this location.
      • Copy the downloaded boot loader binary (boot.bin) and generated application binary (harmony.bin) into the SD card.
      • Insert the SD card into the μSD-CARD connector (J6) on the board.(This connector is present on the bottom face of the board)
      • Reset the board by pressing the Push Button RESET.
    • Press the "START" button to activate board start-up.
    • Insert an SD Card to the SDMMC1 connector(J7).
    • Connect the USB Type-C (USB-A) Connector (J1) on the board to the computer using a USB Type-C cable.
    • RGB LED (D5) turning to Green indicates USB Device Configuration Set Complete event (The USB device functionality has been activated by the USB Host).

    SAM9X75-Curiosity Development Board

    • Setup the SD card (Note: exFAT formatted SD Cards are not supported)
      • Download harmony MPU bootstrap loader from this location.
      • Copy the downloaded boot loader binary (boot.bin) and generated application binary (harmony.bin) into the SD card.
      • Insert the SD card into the μSD-CARD connector (J14) on the board.
      • Reset the board by pressing the Push Button RESET.
    • Press the "START" button to activate board start-up.
    • Connect the USB Micro-B (USB_A) Connector (J2) on the board to the computer using a USB cable.
    • RGB LED (LD1) turning to Green indicates USB Device Configuration Set Complete event (The USB device functionality has been activated by the USB Host).

    SAMA7D65 Curiosity Development Board

    • Setup the SD card (Note: exFAT formatted SD Cards are not supported)
      • Download harmony MPU bootstrap loader from this location.
      • Copy the downloaded boot loader binary (boot.bin) and generated application binary (harmony.bin) into the SD card.
      • Insert the SD card into the SD-CARD connector (J10) on the board.
      • Reset the board by pressing the Push Button RESET.
    • Press the "START" button to activate board start-up.
    • Connect the USB Type-C Connector (J3) on the board to the computer using a USB cable.
    • RGB LED turning to Green indicates USB Device Configuration Set Complete event (The USB device functionality has been activated by the USB Host).

Running the Application

This demonstration uses the selected hardware platform as a logical drive on the computer using the internal Flash of the device as the drive storage media.

Connect the hardware platform to a computer through a USB cable. The device should appear as a new drive on the computer named "Drive Name". The drive can used to store files. The LEDs on the demonstration board will indicate the USB state of the device. Refer to the Configuring the Hardware section for the selected target hardware.

Please note that the user should ensure that the Host is not currently writing data to the media before detaching the device. On a Windows computer before removing the device click on "Safely Remove Hardware" and click on "Eject Media".