1.11 HID Mouse Example (hid_mouse)

This application demonstrates the ability of the MPLAB Harmony USB Device Stack to support HID based two-button mouse device.

Description

This demonstration application creates a USB HID based two-button mouse device. When connected, the device emulates mouse operation by moving the cursor in a circular pattern. When the button in USB device is pressed the movement of cursor is Stopped/Started again .

Downloading and building the application

To clone or download this application from Github, go to the main page of this repository and then click Clone button to clone this repository or download as zip file. This content can also be downloaded using content manager by following these instructions.

Path of the application within the repository is usb_apps_device/apps/hid_mouse.

Following table gives the details of project configurations, target device used, hardware and its IDE. Open the project using the respective IDE and build it.

Project Name IDE Target Device Hardware / Configuration
pic32mz_ef_curiosity_2_0.X MPLABX PIC32MZ2048EFM144 Curiosity PIC32MZ EF 2.0 Development Board
pic32mx470_curiosity.X MPLABX PIC32MX470F512H PIC32MX Curiosity Development Board
sam_e54_xpro.X MPLABX ATSAME54P20A SAM E54 Xplained Pro Board
sam_e54_xpro_freertos.X MPLABX ATSAME54P20A SAM E54 Xplained Pro Board
sam_e70_xult.X MPLABX ATSAME70Q21B SAM E70 Xplained Ultra Board
sam_e70_xult_freertos.X MPLABX ATSAME70Q21B SAM E70 Xplained Ultra Board
pic32cz_ca80_curiosity_ultra.X MPLABX PIC32CZ8110CA80208 PIC32CZ CA80 Curiosity Ultra development board
pic32cx_sg41_curiosity_ultra.X MPLABX PIC32CX1025SG41128 PIC32CX SG41 Curiosity Ultra Evaluation Board
sam_9x75_eb.X MPLABX SAM9X75 SAM9X75-DDR3-EB Evaluation Board

Configuring the Hardware

Curiosity PIC32MZ EF 2.0 Development Board
  • Use the USB micro-B port J201 to connect the USB Device to the USB Host PC.
  • LED1 indicates USB Device Configuration Set Complete event (the USB device functionality has been activated by the USB Host).
  • Use Switch SW1 to stop and start the circular motion of the mouse pointer.
Curiosity PIC32MX470 Development Board
  • Use the USB micro-B port J12 to connect the USB Device to the USB Host PC.
  • LED1 indicates USB Device Configuration Set Complete event (the USB device functionality has been activated by the USB Host).
  • Press the switch S1 to trigger communication from the USB Device to the USB Host.
PIC32CZ CA80 Curiosity Ultra development board
  • Use the USB micro-B "USB DEVICE" connector (J102) to connect the USB Device to the USB Host PC.
  • LED1 indicates USB Device Configuration Set Complete event (the USB device functionality has been activated by the USB Host).
  • Press the switch SW0 to trigger communication from the USB Device to the USB Host.
PIC32CX SG41 Curiosity Ultra Evaluation Board
  • Use the USB micro-B "TARGET USB" connector (J200) to connect the USB Device to the USB Host PC.
  • LED1 indicates USB Device Configuration Set Complete event (the USB device functionality has been activated by the USB Host).
  • Press the switch SW1 to trigger communication from the USB Device to the USB Host.
SAM E54 Xplained Pro Board
  • Use TARGET USB connector on the board to connect the USB Device to the USB Host PC.
  • LED0 indicates USB Device Configuration Set Complete event (the USB device functionality has been activated by the USB Host).
  • Use the Switch SW0 to stop and start the circular motion of the mouse pointer.
SAM E70 Xplained Ultra Board
  • Jumper J203 must be shorted between PB08 and VBUS (positions 2 and 3).
  • Use TARGET USB J200 connector on the board to connect the USB Device to the USB Host PC.
  • LED3 indicates USB Device Configuration Set Complete event (the USB device functionality has been activated by the USB Host).
  • Use Switch SW400 to stop and start the circular motion of the mouse pointer.
SAM9X75-DDR3-EB Evaluation Board
  • Powered the board with an external power supply (or use the micro AB connector).

  • Setup the SD card (Note: exFAT formatted SD Cards are not supported)

    • Download harmony MPU bootstrap loader from this location.
    • Copy the downloaded boot loader binary (boot.bin) and generated application binary (harmony.bin) into the SD card.
    • Insert the SD card into the SDMMC connector (SDMMC0) on the board.
    • Reset the board by pressing the Push Button RESET, then START.
  • Connect the USB Micro-AB Connector on the board to the computer using a micro USB cable.

  • LED near VDDCORE inscription on the board indicates USB Device Configuration Set Complete event (The USB device functionality has been activated by the USB Host).

  • Press the switch USER to stop and start the circular motion of the mouse pointer.

Running the Application

This demonstration uses the selected hardware platform as a USB Mouse. Open the project with appropriate IDE. Compile the project and program the target device.

The LED on the demonstration board will indicate the USB state of the device. Refer to the Configuring the Hardware Section for details.

Before connecting the board to the computer through the USB cable please be aware that the device will begin moving the mouse cursor on the computer. There are two ways to stop the device from allowing the cursor to continue to move. The first way is to disconnect the device from the computer. The second is to press the correct button on the hardware platform. Pressing the button again will cause the mouse cursor to start moving in a circle again.