1.6 CDC Serial Emulator MSD Example (cdc_serial_emulator_msd)

This demonstration application creates a USB composite device that combines the functionality of the cdc_serial_emulator and msd_basic demonstration applications.

Description

This application demonstrates a USB composite device with CDC and MSD functions. The CDC function implements a USB-to-Serial Converter. The MSD function driver implements a USB Mass Storage Device with NVM as storage media.

Downloading and building the application

To clone or download this application from Github, go to the main page of this repository and then click Clone button to clone this repository or download as zip file. This content can also be downloaded using content manager by following these instructions.

Path of the application within the repository is apps\cdc_serial_emulator_msd.

Following table gives the details of project configurations, target device used, hardware and its IDE. Open the project using the respective IDE and build it.

Project Name IDE Target Device Hardware / Configuration
pic32mz_ef_curiosity_2_0.X MPLABX PIC32MZ2048EFM144 Curiosity PIC32MZ EF 2.0 Development Board
pic32cz_ca80_curiosity_ultra.X MPLABX PIC32CZ8110CA80208 PIC32CZ Curiosity Development Board

Configuring the Hardware

Curiosity PIC32MZ EF 2.0 Development Board
  • Use the USB micro-B port J201 to connect the USB Device to the USB Host PC.
  • LED1 indicates USB Device Configuration Set Complete event (the USB device functionality has been activated by the USB Host).
  • The CDC USB (UART to USB) interface on this board is served by the DEBUG_USB connector J700. Connecting this to the PC will create a COM port on the PC Host.
PIC32CZ CA80 Curiosity Ultra development board
  • Use the USB micro-B port J102 to connect the USB Device to the USB Host PC.
  • LED0 indicates USB Device Configuration Set Complete event (the USB device functionality has been activated by the USB Host).
  • The CDC USB (UART to USB) interface on this board is served by the DEBUG_USB connector J200. Connecting this to the PC will create a COM port on the PC Host.

Running the Application

This demonstration functions as a composite USB Device that combines the features of the devices created by the cdc_serial_emulator and the msd_basic demonstration applications. Refer to Running the Demonstration section of the cdc_serial_emulator demonstration and Running the Demonstration section of the msd_basic demonstration for details on exercising the CDC and MSD functions, respectively.

The LEDs on the demonstration board will indicate the USB state of the device, as described in the USB Device State and LED Indication Table in the Device section.