1 Generic Settings
Mounting the SOM on a motherboard requires a specific Pick & Place machine set-up described in the following notes and paragraphs.
For an accurate SOM placement, it is necessary to:
- Position the nozzle in the area defined for module placement on the motherboard using the camera in self-learning mode. The presence of a label will not affect the Pick & Place.
- Define the nozzle type.
- Define speed of movement and other parameters.
Note that the offset from the center is calculated by the machine.
Note: For optimal alignment and
positioning, the nozzle internal diameter should be between 6 and 10 mm. The larger
the nozzle diameter, the better the component alignment and positioning.
Note: In case of non-use of Microchip
tray(s), the tray(s) must be opened under the module to avoid any suction during
module manipulation by the Pick & Place machine.