PIOBUx Alarm Filtering in Static Mode
Filtering the PIOBUx alarm detection is done by programming SECUMOD_PIOBUx.PIOBU_AFV with the value that corresponds to the maximum counter value. See SECUMOD_PIOBUx. The steps are as follows:
- A 9-bit counter is incremented each time the value present on the corresponding input is not the expected one.
- An alarm is sent to the Protection Manager if the counter value reaches the value programmed in PIOBU_AFV.
The 9-bit counter is reset only if the value present on the input is correct and stable for a continuous programmable period defined by SECUMOD_PIOBUx.PIOBU_RFV. Another 9-bit counter is necessary for that operation. See the figure PIOBUx Alarm Filtering Principle.
At reset, the debouncers are not activated (PIOBU_AFV and PIOBU_RFV=0), which implies that no alarm can be generated.
Once both PIOBU_AFV and the PIOBU_RFV are programmed, the corresponding protection is activated and a clear signal is generated automatically when an intrusion is detected.
Instead of clearing the secure memories content, an interrupt or a wakeup signal can be generated. To do so, disable the protection in the Normal Mode Protection register (SECUMOD_NMPR) and configure the Normal Interrupt Enable Protection register (SECUMOD_NIEPR).