12.3.1 Peripherals Security Attribution
Security configurations related to the peripherals are handled by the PAC Controller.
Each peripheral can only be configured either in Secure or in Non-Secure mode except the IDAU peripheral which is always Secured.
The security configuration (Secure or Non-Secure) is propagated to each individual peripheral, thus it is the responsibility of the peripheral to grant or not the access with the following rules:
- If the peripheral is configured
as Non-Secure in the PAC:
- Secure and Non-Secure accesses are granted
- If the peripheral is configured
as Secure in the PAC:
- Secure access is granted
- Non-Secure access is
discarded (Write is ignored, read 0x0), a PAC error is triggeredImportant: These rules do not apply to the specific peripherals called Mix-Secure peripherals.
Note: The Secure application will usually
provide an API for the Non-Secure application using the Non-Secure Callable region (NSC)
to allow the Non-Secure application to request specific resources.
| Mode | Secure Host Access | Non-Secure Host Access |
|---|---|---|
| Non-Secure | Read/Write | Read/Write |
| Secure | Read/Write | Discarded (Write ignored/Read 0x0) PAC Error is generated |
Important: Refer to “Memory
and Peripheral Security Configurations” section for more details on the
programming of NONSECA, NONSECB, and NONSECC parameters.