2.3.3 Group Configuration Masks and Enumerators
It is often required to consult the data sheet to check the bit pattern to be used when setting a bit field to the desired configuration, which also applies when reading or debugging code. Several group configuration masks are defined in the header file to increase the readability and minimize the possibility of setting bits in bit fields incorrectly. Each group configuration mask selects a configuration for a specific group mask.
The name of a group configuration mask is a concatenation of the module type, the bit
field name, a description of the configuration, and a suffix, _gc,
indicating that this is a group configuration. An example of the ADC prescaler
configuration is presented in Figure 2-3.
The group configuration presented in Figure 2-3 sets the prescaler from the peripheral clock (CLK_PER) to the ADC clock with the division factor 4.
The ADC prescaler bit field consists of three bits defining the division factor. The possible configuration names are DIV2, DIV4, DIV8, DIV16, DIV32, DIV64, DIV128, and DIV256. These names make writing and maintaining code very easy, as it requires little effort to understand what configuration the specific mask selects. Table 2-2 shows the available configurations for this bit field.
| PRESC2 | PRESC1 | PRESC0 | Division Factor | Group Configuration Mask |
|---|---|---|---|---|
| 0 | 0 | 0 | CLK_PER divided by 2 | ADC_PRESC_DIV2_gc |
| 0 | 0 | 1 | CLK_PER divided by 4 | ADC_PRESC_DIV4_gc |
| 0 | 1 | 0 | CLK_PER divided by 8 | ADC_PRESC_DIV8_gc |
| 0 | 1 | 1 | CLK_PER divided by 16 | ADC_PRESC_DIV16_gc |
| 1 | 0 | 0 | CLK_PER divided by 32 | ADC_PRESC_DIV32_gc |
| 1 | 0 | 1 | CLK_PER divided by 64 | ADC_PRESC_DIV64_gc |
| 1 | 1 | 0 | CLK_PER divided by 128 | ADC_PRESC_DIV128_gc |
| 1 | 1 | 1 | CLK_PER divided by 256 | ADC_PRESC_DIV256_gc |
The bit group configuration is typically used in conjunction with the bit group mask to first ensure clearing the old configuration to change a bit field to a new configuration.
Unlike bit masks and group masks, the bit group configuration masks are defined using C enumerations. One enumeration is defined for each bit field. The code below shows the enumeration for the USART CMODE bit field.
typedef enum USART_CMODE_enum
{
USART_CMODE_ASYNCHRONOUS_gc = (0x00<<6), /* Asynchronous mode */
USART_CMODE_SYNCHRONOUS_gc = (0x01<<6), /* Synchronous mode */
USART_CMODE_IRCOM_gc = (0x02<<6), /* Infrared communication */
USART_CMODE_MSPI_gc = (0x03<<6), /* Host SPI mode */
} USART_CMODE_t;
The name of the enumeration is a concatenation of the module type (USART), the bit field
(CMODE), and a suffix (_enum).
Figure 2-4 presents the naming convention.
Each of the enumeration constants behaves much like an ordinary constant when used on its
own. However, using an enumeration type definition has the advantage of creating a new
data type. The name of the data type, for this example, is
USART_CMODE_t. A USART_CMODE_t variable can be
used directly as an integer, but assigning an integer to an enumeration type will
trigger a compiler warning, which can be used to the programmer’s advantage.
Any legal or illegal value can, for example, be passed to the function if a function that
sets the communication mode for a USART module accepts the communication mode as an
integer type (for example, unsigned char). Only the four predefined
constants in the USART_CMODE_t enumeration type can be passed to the
function if the function instead accepts a parameter of type
USART_CMODE_t. Passing anything else will result in a compiler
warning.