1.15 SPI Driver Asynchronous - Self-Loopback Multi Client

This example demonstrates how to use the SPI driver in Asynchronous mode to achieve self-loopback between multiple clients.

Description

  • This example writes and reads back the same data (self-loopback) for two different clients connected over the same SPI bus by using the multi-client feature of the driver
  • It uses the request (write and read request) queuing feature of the asynchronous driver and does not waste CPU bandwidth in waiting for previous request completion
  • The example also demonstrates how to setup two different client transfers at different baud rates
  • This example performs self-loopback only once after a power-on reset
  • Success is indicated when a successful self-loopback is reported by both the clients
  • After the loop back test is complete, the application remains in the Idle state

Downloading and Building the Application

To clone or download this application from GitHub, go to the main page of this repository and then click Clone button to clone this repository or download as zip file. This content can also be downloaded using content manager by following these instructions.

Path of the application within the repository is apps/driver/spi/async/spi_self_loopback_multi_client/firmware.

To build the application, refer to the following table and open the project using its IDE.

Project NameDescription
pic32mz_ef_sk.XMPLAB X project for PIC32MZ Embedded Connectivity with FPU (EF) Starter Kit

Setting Up the Hardware

The following table shows the target hardware for the application projects.

Project NameDescription
pic32mz_ef_sk.XPIC32MZ Embedded Connectivity with FPU (EF) Starter Kit

Setting Up PIC32MZ Embedded Connectivity With FPU (EF) Starter Kit

  • Connect the Debug USB port on the board to the computer using a mini USB cable
  • Use a jumper wire to connect Pin 7 of J12 to Pin 37 of J12
    • SDI3 is mapped to RA14, which is routed to Pin 7 of J12
    • SDO3 is mapped to RD10, which is routed to Pin 37 of J12