1 Harmony 3 Driver and System Service Application Examples for PIC32MZ EF Family
The following applications are provided to demonstrate the typical or interesting usage models of one or more drivers and system services.
| Name | Description |
|---|---|
| Console Debug System Service Using UART | This example application demonstrates the UART based console and debug system service |
| Console Debug System Service Using USB | This example application demonstrates the USB based console and debug system service |
| EEPROM Emulator Library Read/Write | This application example demonstrates how to read and write to the Emulated EEPROM memory space using the EEPROM Emulator library |
| FAT File System Using NVM and SDSPI Media | This application shows an example of using the MPLAB Harmony File System to access files across multiple media (NVM, SDSPI) |
| FAT File System Using NVM and SST26 Media | This application shows an example of using the MPLAB Harmony File System to access multiple files across multiple media (NVM, SQI Flash) |
| FAT File System Using NVM Media | This application shows an example of implementing a FAT disk in the device internal Flash memory |
| FAT File System Using SDSPI Media | This application shows an example of using the MPLAB Harmony File System to access and modify the contents of an SD card using the SDSPI driver and the SPI PLIB |
| FAT File System Using SST26 Media | This application shows an example of using the MPLAB Harmony File System to access SQI based SST26 Flash media |
| FreeRTOS Basic | This example application demonstrates context switching between four tasks of different priorities. Two tasks run periodically while the other two tasks are event driven |
| FreeRTOS Task Notification | This example application is to illustrate the FreeRTOS Task Notification feature which is used as a lightweight binary semaphore |
| Memory Driver Asynchronous - NVM SST26 Read/Write | This example application shows how to use the Memory driver in Asynchronous mode to perform block operations on the NVM and the SST26 media |
| Memory Driver Synchronous - NVM SST26 Read/Write | This example application shows how to use the Memory driver in Synchronous mode to perform block operations on the NVM and the SST26 media |
| MPFS File System Using NVM Media | This application shows an example of implementing an MPFS disk in device internal Flash memory |
| SDSPI Driver Synchronous - SDSPI Read/Write | This example application shows how to use the SDSPI driver in Synchronous mode to perform block operations on the SD card media |
| SPI Driver Asynchronous - Self-Loopback Multi Client | This example demonstrates how to use the SPI driver in Asynchronous mode to achieve self-loopback between multiple clients |
| SPI Driver Synchronous - Self-Loopback Multi Client | This example demonstrates how to use the SPI driver in Synchronous mode to achieve self-loopback between multiple clients in RTOS environment |
| SQI Flash SST26 Driver - SST26 SQI Read/Write | This example application shows how to use the SST26 driver to perform block operations on the on-board SST26 Flash memory in Quad IO mode |
| Time System Service Multi Client | This example application demonstrates the multi-client system timer functionality |
| USART Driver Asynchronous - USART Echo | This example echoes the received characters over the console using the USART driver in Asynchronous mode |
| USART Driver Synchronous - USART Echo | This example echoes the received characters over the console using the USART driver in Synchronous mode |