1.12 Memory Driver Synchronous - NVM SST26 Read/Write

This example application shows how to use the Memory driver in Synchronous mode to perform block operations on the NVM and the SST26 media.

Description

  • Uses multi instances of the Memory driver to communicate with the NVM and the SST26 Flash memories in Synchronous mode of operation in RTOS environment
  • Performs block Erase/Write/Read operations on both the media
  • Consists of three tasks which are called in the RTOS thread context:
    1. APP_SST26_Tasks():
      • Performs operations on the SST26 QSPI/SQI Flash memory
    2. APP_NVM_Tasks():
      • Performs operations on the NVM
    3. APP_MONITOR_Tasks():
      • Monitors the state of above two Tasks

Downloading and Building the Application

To clone or download this application from GitHub, go to the main page of this repository and then click Clone button to clone this repository or download as zip file. This content can also be downloaded using content manager by following these instructions.

Path of the application within the repository is apps/driver/memory/sync/nvm_sst26_read_write/firmware.

To build the application, refer to the following table and open the project using its IDE.

Project NameDescription
pic32mz_ef_sk_freertos.XMPLAB X project for PIC32MZ Embedded Connectivity with FPU (EF) Starter Kit

Setting Up the Hardware

The following table shows the target hardware for the application projects.

Project NameDescription
pic32mz_ef_sk_freertos.XPIC32MZ Embedded Connectivity with FPU (EF) Starter Kit

Setting Up PIC32MZ Embedded Connectivity With FPU (EF) Starter Kit

  • Connect the Debug USB port on the board to the computer using a mini USB cable